×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109763301, Entry date: 10/13/2017
(0)
Rate

Information and updates for block library Migration SIMOCODE pro for SIMATIC PCS 7 version V9 or V8 without Advanced Process Library (APL)

  • Entry
  • Associated product(s)
Download of service packs and hotfixes and information about versions of the SIMOCODE pro block library for SIMATIC PCS 7.

Ordering data of the block library

3UF7982-0AA20-0 Engineering software Migration V7-V9 / Engineering software Migration V7-V8
3UF7982-0AA10-0 Engineering software V7
3UF7982-0AA11-0 Runtime license V7.X (Runtime license of predecessor version is to be used)

Information for other SIMOCODE pro block libraries for SIMATIC PCS 7 see 109760422 


Version, Service Pack (SP), Hotfix (HF):

Always use the latest versions.

Check compatibility 64847781 

Correlation between the name of the Engineering software and the version number of the SIMOCODE pro block library Migration:

Engineering software Migration V7-V8 corresponds to
  block library Migration SIMOCODE pro V8.0 to V8.0 + SP1

Engineering software Migration V7-V9 corresponds to
  block library Migration SIMOCODE pro V8.0 + SP2 (or higher)

Engineering software Migration V7-V9 can be used for the following migration scenarios:
  V7-V9, V8-V9, V7-V8


Engineering software Migration V7-V9
Library Migration V8.0 + SP2
 

a) Type of delivery: CD. Article No. 3UF7982-0AA20-0

Requirement for installation of the CD version:
If a previous version (Engineering software Migration V7-V8 / V7-V9 / Migration V8.0 or higher) is already installed on your system, it has to be uninstalled manually before starting the setup. The parallel installation of both libraries is not possible. SIMOCODE pro block library V7-V9 Migration V8.0+SP2 includes complete functionality of the previous library.

b) Type of delivery: Download. 109751173

Requirement for installation of the Download version:
The installation of the SIMOCODE pro block library Migration V8.0+SP2 (download version) requires the existing installation of a previous version (Engineering software Migration V7-V8 / V7-V9 / block library Migration V8.0 or higher) and can be installed directly. In this case, the installer will replace the existing files.


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.