×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109763384, Entry date: 09/25/2019
(1)
Rate

SICAM GridPass V1.30 Software

  • Entry
  • Associated product(s)
SICAM GridPass is an easy to manage PKI (public key infrastructure) product which creates and manages X.509 standardized certificates. SICAM GridPass offers also a CRL distribution point as http webserver and a EST server (Enrollment over Secure Transport) for automated certificates enrollment. GridPass is https based and can be managed over a Chrome browser.

SICAM GridPass V1.30 ISO Image. The Software can be used for updating an older one with a valid license key or can be used without a license key as Trial version under the Siemens Software license conditions for "Trial License".

Please note that the Trial License is ONLY for testing purposes and the period of usage is limited to 120 days and commences with the SW start-up. Every data produced with this product are also licensed under this Trial License conditions. Generated CA certificates have a fixed validity period of 90 days for SICAM GridPass installations having no installed license file (ALM)

SICAM GridPass full and trial version download (registration required):

 Download unterliegt Exportcontrolle  SICAM_GridPass_V1.30.iso (215,8 MB)

SICAM GridPass manual download page:

SICAM GridPass V01.30 Manual

SICAM GridPass Release Notes download page:

Release Notes V1.30

SICAM GridPass Software Product Sheet download:

  SICAM_GridPass_SoftwareProductSheet.pdf (838,5 KB)


Terms of Use

Reservation regarding future software downloads

The Software offered for download is currently provided free of charge (under considering of the valid license conditions). For the future, Siemens reserves the right to provide the Software against payment of a royalty fee.

General License Conditions

General License Conditions Software

Third Party Software - Terms of License and Copyright

Among other things, this product contains Open Source Software that was developed by third parties. The Open Source Software included with this product and the relevant Open Source Software license agreement can be found in Readme_OSS. The Open Source Software program is protected by copyright. You are permitted to use the Open Source Software according to the Open Source Software license agreement.
You can download the Readme_OSS file here:

 Registrierung notwendig  Readme_OSS_V1.30.html (864,6 KB)

Special Information for Resellers

The information and the license terms in the Readme_OSS file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

Disclaimer regarding use of previous software versions

Siemens’ products and solutions undergo continuous development to remain leading in many fields of technology and to represent the state of the art. Siemens strongly recommends to apply product updates as soon as available and to always use the latest product versions.

Use of product versions that are no longer supported, and failure to apply latest updates may increase customer’s exposure to system degradation. By downloading unsupported product version the customer confirms that he operates this outdated product version at his own risk and responsibility and with full awareness of potential risks and consequences and confirms his conscious decision to abandon the enhancements available only with the current version as listed in [1]. The customer has read that he should actively plan the upgrade of his installed base to the latest supported product versions.

The Customer hereby explicitly agrees and accepts that Siemens does not cover any warranty or liability, explicitly or implicitly, regardless of any legal reason, for any damages or losses caused directly or indirectly by the use of outdated/unsupported product versions.
The Customer shall indemnify and hold Siemens harmless against any third-party claims existing or arising in this connection.

[1] Further information about Siemens ProductCERT and Siemens CERT

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.