×
Siemens Industry Online Support
Siemens AG
Type de contribution : FAQ ID de la contribution : 109763454, Date de la contribution : 14/02/2019
(1)
Évaluer

Which user authorizations do you need to be able to collect hardware information with the SAS-DC (SIMATIC Assessment Suite - Data Collector)?

  • Contribution
  • Concerne le/les produits(s)
Read out device and diagnostics information
The SAS-DC (SIMATIC Assessment Suite - Data Collector) enables you to execute a project export of a STEP 7 project in order to read out the device and diagnostics information.
In order for the acquisition of automation component data via the STEP 7 interface to function you have to fulfill the following requirements in the Windows operating system.

Requirements

  • The storage paths of the STEP 7 project and the SAS-DC in the Windows Explorer must not be longer than 120 characters.
  • The STEP 7 project must be stored and processed with the same user as the one with which you want to start the SAS-DC.
  • Even if the user has administrator authorization, the STEP 7 instance cannot access the projects that have not been created and processed by that user.
  • The project must have been opened at least once by the user in the SIMATIC Manager. By doing so the project is in the user's list and it is possible to collect the STEP 7 project data.
  • When using the SAS-DC you should always log on as local administrator. This can also be in a domain.
  • The user who executes the SAS-DC must be member of the user groups "SIMATIC HMI" and "SIMATIC NET".

Further Information

  • How do you efficiently collect diagnostics and system information? 65976201
  • SIMATIC Remote Services - "Preventive" module: How do you collect device and diagnostics information with the SAS DC? 109485717
Notes relatives à la sécurité
La protection des installations, systèmes, machines et réseaux contre les cyber-menaces nécessite la réalisation (et le maintien continu) d'un concept global de sécurité IT à la pointe de la technique. Les produits et solutions Siemens ne constituent qu'un élément d'un tel concept. Pour plus d’informations sur la cyber-sécurité, rendez-vous sur
https://www.siemens.com/cybersecurity#Ouraspiration.
Aide pour la statistique
Cette fonction permet de délivrer les identifiants des résultats de la recherche selon la quantité souhaitée (format .txt).

Générer une liste
Copier l'URL
Afficher cette page dans le nouveau design
Poste de commande mySupport