×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109763893, Entry date: 05/28/2019
(3)
Rate

Updates for TIA Portal Multiuser Server V15.1

  • Entry
  • Associated product(s)
Status 05 / 2019 : Update 2

These updates are valid for the following products in the TIA Portal

  • TIA Portal Multiuser Engineering V15.1 (Server)


Installation instructions: 

  • The updates are cumulative and contain all previous updates.
  • The update can only be installed if one of the products mentioned above is already installed


You can find updates for STEP 7 V15.1 in the following entry 109763890


You can find updates for WinCC Runtime Advanced V15.1 in the following entry 109763891 

You can find updates for WinCC Runtime Professional V15.1  in the following entry 109763892

You can find updates for SIMATIC Energy Suite V15.1  in the following entry 109763894

You can find updates for Migration Tool TIA V15.1  in the following entry 58638200 

_______________________________________________________________________________

Update 1 (02/2019)

Improvements compared to earlier versions:

  • The availability of the multiuser server has been improved for a larger number of non-current local sessions for a server project.

Update 1 for TIA Portal Multiuser Engineering V15.1 (Server):

 Download unterliegt Exportcontrolle  TIA_Portal_Multiuser_Server_V15_1_Upd1.exe (124,2 MB)

SHA-256 checksum:

 Download unterliegt Exportcontrolle  TIA_Portal_Multiuser_Server_V15_1_Upd1.txt (1 KB) Information on SHA-256

_______________________________________________________________________________

Update 2 (05/2019)

Improvements compared to earlier versions:

  • The stability when working with the multiuser server has been improved based on customer feedback, among other things.

Update 2 for TIA Portal Multiuser Engineering V15.1 (Server):

 Download unterliegt Exportcontrolle  TIA_Portal_Multiuser_Server_V15_1_Upd2.exe (124,4 MB)

SHA-256 checksum:

 Download unterliegt Exportcontrolle  TIA_Portal_Multiuser_Server_V15_1_Upd2.txt (1 KB) Information on SHA-256

_______________________________________________________________________________

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.