×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109763898, Entry date: 02/11/2019
(7)
Rate

SIMOCODE ES V15.1 (TIA Portal)

  • Entry
  • Associated product(s)
The central software package for the configuration, commissioning, operation, and diagnosis of SIMOCODE pro.

SIMOCODE ES V15.1 is the central software package for the configuration, commissioning, operation, and diagnosis of SIMOCODE pro.

Licenses for SIMOCODE ES V12 / V13 / V14 / V15 are also suitable for SIMOCODE ES V15.1.

SIMOCODE ES V15.1 and SIMOCODE ES V15 have identical article-numbers.

The software is based on the Totally Integrated Automation Portal (TIA Portal) central engineering framework and can be seamlessly integrated if additional TIA Portal-V15.1-based software such as STEP 7 and WinCC is present, thus providing the user with a consistent, efficient, and intuitive solution to all automation tasks.
But those using SIMOCODE ES V15.1 as standalone software will also enjoy its benefits.

SIMOCODE ES V15.1 can be installed side-by-side to SIMOCODE ES V15.


What is new in SIMOCODE ES V15.1 compared with V15? 

Folgende Neuheiten stehen bei SIMOCODE ES im TIA Portal zur Verfügung:

  • Direct support of the following new SIMOCODE pro modules:
  • SIMOCODE pro V PN V2.1 basic unit with ATEX dry-running protection
  • SIMOCODE pro V PN GP V2.1 basic unit (PROFINET General Performance devices)
  • Current/voltage measuring module IUM V2 DRP with ATEX dry-running protection

  • Access to all device-specific parameters via the TIA Openness interface:
    • Creating and configuring SIMOCODE pro devices via the Openness interface

    • Offline determination of all SIMOCODE pro parameters

    • Networking of devices

    • Support of export and import of CAx data

    • Support of export and import of one/several device(s) to an AML file/from an AML file


You will find detailed information on this in the online help for SIMOCODE ES V15.1 topics "Openness - Fundamentals" and "Overview of the device-specific SIMOCODE pro Openness attributes".

  • SIMOCODE pro V PN enables dry-running protection of centrifugal pumps (non-electrical device) by active power monitoring and motor shutdown. This applies to centrifugal pumps with progressive flow characteristics, which are also suitable for pumping flammable media and are also installed in hazardous areas. You will find detailed information on this in the online help for SIMOCODE ES V15.1 topics "Dry-running protection of centrifugal pumps by active power monitoring" and "Dry-running protection wizard".

  • The following inscription parameters can now be changed online during operation.

    • Plant identifier

    • Location designation

    • Installation date

    • Description 


Three program versions

The user can choose between three different versions of SIMOCODE ES: SIMOCODE ES Basic, SIMOCODE ES Standard, and SIMOCODE ES Premium.
New: Since V15, SIMOCODE ES Basic SIMOCODE as a powerful tool for commissioning or maintenance engineers is offered for download free of charge at Siemens Industry Online Support using this download entry-ID.

SIMOCODE ES Standard and Premium, with their more extensive range of functions and integrated graphics editor, are perfect tools for engineering and configuring. Unlike the Standard version, SIMOCODE ES Premium also permits parameterization and diagnostics through PROFIBUS/PROFINET. The display of all operating, service, and diagnostics data supplies important information about the current state of the motor and plant at all times – everywhere on PROFIBUS or PROFINET


Integrated graphics editor

The graphics editor is a part of SIMOCODE ES Standard and SIMOCODE ES Premium. It is based on the Continuous Function Chart (CFC) and adds a powerful tool to the parameterizing interface that enables easy parameterization of devices by Drag&Drop. Extremely compact documentation of all configured parameters is possible, as is the graphic online presentation of the configured device functions including all signal states during operation.


Trial License

The software comprises a trial license of SIMOCODE ES V15.1 Premium. The Licensee shall be granted the non-exclusive and non-transferable right to install the SW in one (1) Instance and to use it for validation purposes in the manner specified in the Order Data or CoL (see "Type of Use"). The period of usage is limited to 21 days and commences with the SW start-up, unless a different period of usage is specified in the Order Data or CoL.


System requirements 

Operating system

Windows 7 64 Bit Professional/Ultimate/Enterprise (Service Pack1) 
Windows 10 64 Bit Pro/Enterprise 1709/1803/1809
Windows 10 64 Bit Enterprise 2016 LTSB
Windows Server 2012 R2 StdE (full installation)
Windows Server 2016

Processor
recommended
minimum


Intel ® Core™ i5-6440EQ (up to 3.4 GHz)

Intel® Core™ i3-6100U, 2.30 GHz

RAM
recommended
minimum


16 GB or more (32 GB for large projects)
4 GB

Monitor
recommended
minimum
 

15.6" Full HD Display (1920 x 1080 or higher)
1024 x 768

Hard disc
recommended
minimum

SSD with at least 50 GB available memory space
S-ATA with at least 8 GB available memory space

CD-ROM-/DVD drive

DVD-ROM (only when installing from DVD)

Interface

depending on PC cable type: serial (COM) or USB

PC cable/parameterization cable/connection cable

Yes, USB

PROFIBUS interface

Optional, for parameterization and diagnostics via PROFIBUS

Ethernet interface

Optional, for parameterization and diagnostics via Ethernet/PROFINET


Third-party software - Licensing terms and copyright information

You can find the copyright information for third-party software contained in this product, particularly open source software, as well as applicable licensing terms of such third-party software in the ReadMe_OSS file.

Special information for resellers

The information and the license terms in the ReadMe_OSS file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

 Registrierung notwendig  Readme_OSS.zip (2,9 MB) 


Installation notes

Please first download the file “SIRIUS_SIMOCODE_ES_V15_1.exe” and then execute it. Afterwards, the file will be extracted and you can execute the setup.

  Installation notes (124,9 KB) 


Download (also contains OSS source code)

 Registrierung notwendig  SIRIUS_SIMOCODE_ES_V15_1.exe (2,3 GB)

SHA-256 checksum:   Registrierung notwendig  Code_SIRIUS_SIMOCODE_ES_V15_1.txt (1 KB)
Information about SHA-256:  109483101



Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.