×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109763972, Entry date: 03/28/2019
(0)
Rate

Hotfix 1 (HF1) for SIMATIC Modbus/TCP CP Red V3 (6AV6676-6MB30-3AX0 / 6AV6676-6MB30-3AD0)

  • Entry
  • Associated product(s)
Version: 01/2019: Hotfix 1

This update is valid for the following product as from Step 7 V5.4:

  • SIMATIC Modbus/TCP CP Red V3       6AV6676-6MB30-3AX0

                                                                       6AV6676-6MB30-3AD0

 

Contents:

  • MB_REDCL V3.1
  • MB_CPCLI V2.4

 

What's new?

  • The block correctly restarts following a CPU restart
  • In case of protocol errors, the connection status is displayed correctly

 

Installation:

  • Unpack the library.
  • Copy the Client blocks from the relevant folder into the user project.
  • Load  the modbus blocks and the empty instance DB of the modbus block into the CPU.
  • Initialize the block with the init bit or restart the CPU.


 

 Registrierung notwendig  Hotfix1_CP_Red_V3.zip (158.9 KB)

 Registrierung notwendig  hashMD5.txt (1 KB)


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.