×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109764302, Entry date: 03/06/2019
(0)
Rate

SIMOTION P320-4: Why are the keys for Restart, Terminate, etc. grayed out and can no longer be operated?

  • Entry
  • Associated product(s)
For SIMOTION P you need the setting "Never report" of the user account control.

With the setting of the User Access Control or UAC you can define in Windows 7 for which actions that require administrator rights a confirmation is necessary. For SIMOTION P you need the setting "Never report".

Sometimes installation programs (the IPC Wizard, for example) make changes to the security settings of Windows and change the setting of the User Access Control.
Therefore, after installing programs or updates, you should check the setting of the User Access Control and, if necessary, reset it to "Never report". 

If "Never report" is not set for the User Access Control, the keys for Restart, Terminate, etc. are grayed out and can no longer be operated.

Further information about the User Access Control in Windows 7 is available, for example, in the Microsoft Support

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.