×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109764381, Entry date: 03/06/2019
(0)
Rate

HF1 for Drive ES PCS7 APL V8.2 SP2

  • Entry
  • Associated product(s)
You can download Hotfix 1 for the Drive ES PCS7 APL V8.2 SP2 software here.

Hotfix 1 eliminates the following malfunctions:
SIEMENS drive units (MICROMASTER 4, SINAMICS) are configured behind the Y link.  When compiling CFCs with the module driver, certain nodes are not automatically connected. 
After installing Hotfix 1, the error no longer occurs when compiling CFCs with the module driver.

Hotfix 1 also expands the necessary information for using the PCS 7 module driver with the following new SINAMICS devices:

  • SINAMICS G120X (configuration only via GSD/GSDML)

  • SINAMICS G130 V5.2

  • SINAMICS G150 V5.2

  • SINAMICS S120 V5.2

  • SINAMICS S150 V5.2


Hotfix 1 is available in two installation versions.

Hotfix 1 for drive ES PCS7 APL V8.2 SP2 (single license):
Installation requirement:

Drive ES PCS7 APL V8.2 SP2 is not installed in the upgrade license. Please use the following Hotfix 1 installation package:

Procedure for installing the HF1 on Drive ES PCS7 APL V8.2 SP2:

  1. Download the attached ZIP file "HF1_DriveES_PCS7_APL_V82_SP2.zip".
  2. Unzip the zip file to a target directory on your hard disk. Please make absolutely sure that there are no spaces anywhere in the path name of the target directory.
  3. After unpacking, the shared directory must appear as follows:
    \...\InstData\
    \...\Readme\
    \...\Setup.exe, .....
  4. Start the Hotfix setup program by calling …\Setup.exe

You can find more information on Drive ES PCS7 APL V8.2 SP2 itself under the entry ID: 109755489.

 Registrierung notwendig  HF1_DriveES_PCS7_APL_V82_SP2.zip (8.3 MB) 

Checksum:   Registrierung notwendig SHA512.txt (1 KB)

Information on SHA-512: 109483101 


Hotfix 1 for Drive ES PCS7 APL V8.2 SP2 upgrade license:
Installation requirement:

Drive ES PCS7 APL V8.2 SP2 is installed as an upgrade license. Please use the following Hotfix 1 installation package:

Procedure for installing the HF1 on Drive ES PCS7 APL V8.2 SP2:

  1. Download the attached ZIP file "HF1_DriveES_PCS7_APL_V82_SP2_upgrade.zip".
  2. Unzip the zip file to a target directory on your hard disk. Please make absolutely sure that there are no spaces anywhere in the path name of the target directory.
  3. After unpacking, the shared directory must appear as follows:
    \...\InstData\
    \...\Readme\
    \...\Setup.exe, .....
  4. Start the Hotfix setup program by calling …\Setup.exe

You can find more information on Drive ES PCS7 APL V8.2 SP2 itself under the entry ID: 109755489.

 Registrierung notwendig  HF1_DriveES_PCS7_APL_V82_SP2_upgrade.zip (8.3 MB)

Checksum:  Registrierung notwendig  upgr_SHA512.txt (1 KB)



Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.