×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109764416, Entry date: 02/20/2019
(1)
Rate

Download of Firmware SCALANCE M-800 / S615 V06.01

  • Entry
  • Associated product(s)
This firmware update V06.01 can be used for SCALANCE M812, M816, M826, M804PB, M874-x, M876-x and S615 products and replaces the older firmware versions. You can find additional information on downloading new firmware in the configuration manual ID: 109751632

Affected MLFBs:

Product name

Order number

SCALANCE M804PB

6GK5804-0AP00-2AA2

SCALANCE M812-1 (ANNEX A)

6GK5812-1AA00-2AA2

SCALANCE M812-1 (ANNEX B)

6GK5812-1BA00-2AA2

SCALANCE M816-1 (ANNEX A)

6GK5816-1AA00-2AA2

SCALANCE M816-1 (ANNEX B)

6GK5816-1BA00-2AA2

SCALANCE M826-2

6GK5826-2AB00-2AB2

SCALANCE M874-2

6GK5874-2AA00-2AA2

SCALANCE M874-3

6GK5874-3AA00-2AA2

SCALANCE M876-3

6GK5876-3AA02-2BA2

SCALANCE M874-3 (CN)

6GK5874-3AA00-2FA2

SCALANCE M876-3 (ROK)

6GK5876-3AA02-2EA2

SCALANCE M876-4 (EU)

6GK5876-4AA00-2BA2

SCALANCE M876-4 (NAM)

6GK5876-4AA00-2DA2

SCALANCE S615

6GK5615-0AA00-2AA2

RUGGEDCOM RM1224 LTE(4G) EU

6GK6 108-4AM00-2BA2

RUGGEDCOM RM1224 LTE(4G) NAM

6GK6 108-4AM00-2DA2

 

1. Reason for change:

New functions:

  • Uwer-specific firewall

    • Firewall rules can be activated or deactivated dynamically, depending on the user

    • This allows to ensure or restrict the access to plant / system parts

  • Secure SMTP

  • Secure NTP Server

  • SINEMA RC Fallback Fingerprint on KEY PLUG

  • SIM Handling

    • Change PIN

    • disable/enable PIN

    • unlock SIM using PUK

  • Secure Events

  • Performance Improvements M804PB

  • M804PB configuration parameters

    • The configuration parameters are now also available after restart

  • NETMAP revisions

    • Auto firewall rules for NETMAP rules

    • Bidirectional creation of NETMAP rules

    • NETMAP rules can be edited in WBM

  • Change of the “default admin” name

  • Increase of the maximum of DHCP Server pools  from 5 to 8

  • Safe protocols in factory settings (“DCP Server read only“ after the first configuration)

  • Daylight saving time

  • DHCP keep-alive can be deactivated (S615 via WBM or CLI, other devices via CLI only)

Corrections:

  • Minor improvements and corrections

  • OSS updates and security updates

  • Improvements regarding SMS

  • Improvements regarding IPSec

  • Improvements regarding the connection of SCALANCE M804PB and Cloud Connector

Security information:

  • This update includes security-related changes. We therefore recommend that you update the firmware.


    2. Important note on firmware update via WBM or SINEMA RC

    A firmware update to version V06.01 from version V04.03 / V04.03.01 only works if the "Firmware on PLUG" function is disabled prior to upgrading the firmware. Make sure that the feature is disabled prior to the update (System->PLUG->Firmware on PLUG).

    If the feature is still enabled during the firmware update, the firmware will be rejected.


    3. Important note on the C-PLUG 6GK1900-0AB00 (affects products as of delivery date  November 2017) and SCALANCE M-800 / S615 Firmware Version < V5.0

    With a plugged C-PLUG 6GK1900-0AB00 that was delivered in November 2017 or later, a software restart (e.g. via WBM, reset button, automatically following a firmware update, etc.) of a SCALANCE M800/S615 may result in problems.

    A restart is required after a firmware update, which is why we advise you not to perform an update via remote access in this special case. You run the risk of not being able to access the SCALANCE M800/S615 any longer. To rectify the error, the device must be briefly disconnected from power (action on site required).

    The C-PLUG 6GK1900-0AB00 should therefore ot be used with a SCALANCE M800/S615 software version prior to V5.0. We recommend that you use a KEY-PLUG SINEMA RC.

    The KEY-PLUG SINEMA RC is not affected by this problem.

    SCALANCE M800/S615 devices that were delivered with firmware version V5.0 (or higher) are not affected by this problem.

    The serial numbers of the affected C-PLUGs start with:

    • SVP JN

    • SVP JD

    • SVP K1

    • SVP K2

    • SVP K3

    • SVP K3

    • SVP K4

    • SVP K5

    In addition, a restart via the hardware SET button with a plugged affected C-PLUG can result in problems. This is why, for SCALANCE M800/S615 devices that were delivered before May 2018, the SET button is not supported with the C-PLUGs described above.



    4. Description of the download procedure:

    For the SCALANCE M804PB, SCALANCE M81x, SCALANCE M826, SCALANCE M874-x, SCALANCE M876-x and SCALANCE S615 devices, you can download the software free of charge as the file "firmware_enc_sig_trustcenter_OSS.zip". Double-clicking on this file extracts the following files:

    Update file:
    firmware_enc_sig_trustcenter.sfw

    OSS information:
    OSS_SCALANCE_M-800_S615_86.htm


    Third-party software – license conditions and copyright information

    You can find copyright information for the third-party software contained in this product, particularly Open Source Software, as well as applicable license conditions of such third-party software in the OSS_SCALANCE_M-800_S615_86.htm file.

    Special note for resellers

    The information and the license conditions stated in the OSS_SCALANCE_M-800_S615_86.htm file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

      OSS_SCALANCE-M-800-S615_86.pdf (16.6 MB)


    You can download the zip files here:

     Registrierung notwendig  firmware_enc_sig_trustcenter_OSS.zip (36.5 MB)



    5. Description of the update procedure:

    Then open the "System" folder in the web interface of the corresponding SCALANCE M-800 product and click "Load&Save". In the "Firmware" row, the file "firmware_enc_sig_trustcenter.sfw" can then be imported by clicking "Load". After the firmware has been successfully loaded into the SCALANCE M-800 / S615 product, you need to perform a restart. You can find additional information on downloading new firmware in the configuration manual 109751632 

     

    6. SCALANCE M804PB - Download TIA Portal Cloud Connector

    For optimal use of the SCALANCE M804PB it is recommended to install the latest version of the TIA Portal Cloud Connector (V1.1 SP3 Update 1). 

    Improvements compared to earlier versions:

    • meassurements to improveme the communication performance with a SCALANCE M800

    • improvement of the stability of the communication with a SCALANCE M800 

    Here you can download the file: 109764115 


    Downgrade and previous versions:

    For security reasons, we do not recommend downgrading or using older firmware versions. However, if you need a previous version, please contact Technical Support.