×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109765124, Entry date: 04/16/2019
(1)
Rate

How do you configure and diagnose the SCALANCE W devices via SNMP?

  • Entry
  • Associated product(s)
The SCALANCE W devices can be configured and diagnosed with SNMP. This document describes frequently used OIDs to adapt various options.

Description
The SCALANCE W devices can be configured and diagnosed with SNMP. This document describes frequently used OIDs to adapt various options.

Document contents
The following options are dealt with in the document:

  • Set the SSID in the Client
  • Activate Channels via the Allowed Channel List
  • Enable and Disable the Radio Interface
  • Change the Operating Mode at the Access Point
  • Change the SSID at the Access Point
  • Set the Channel at the Access Point
  • Start the Scan Procedure for Roaming via SNMP
  • Control digital output via SNMP
  • Read Out Client List at the Access Point
  • Acquire Single Information Items of a Client
  • Read Out Available AP List on the Client
  • Acquire Single Information Items from the Available AP List
  • Read Out Overlap AP List at the Access Point
  • Acquire Single Information Items from the Overlap AP List

 Each option is explained in detail in a separate chapter and you will be shown how you have to use and change the OIDs.

Download
  Documentation (955,1 KB)

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.