×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109765183, Entry date: 03/07/2019
(0)
Rate

Update of the EK-ERTEC 200P with ERTEC 200P-2 to firmware V4.6

  • Entry
  • Associated product(s)
A new firmware with extended functions is provided for the ERTEC 200P Evaluation Kit for the development of a PROFINET device.

The Evaluation Kit ERTEC 200P is used for the development of a PROFINET device.

The firmware stack included in the scope of delivery can be operated both on the ERTEC 200P and on the ERTEC 200P-2.

New features of V4.6 compared to V4.5

The firmware stack for the EK-ERTEC 200P contains the following new functionalities from version 4.6 onwards:

  • Support of Asset-Management-Record (AMR)
  • Support of R+H Sync
  • Configuration in Run (CiR) as device functionality
  • HW example for coupling the ERTEC 200P-2 to a host processor via XHIF interface

The firmware stack V4.6 can be downloaded via the attached link.
 Registrierung notwendig  EK200P46.zip (1,4 GB) 

A password is required to unzip the file. Registered customers will receive the password from the ComDeC.
comdec@siemens.com 

---------------------------
Checksum information : ( How do you determine the SHA-256 checksum of a file? : 109483101 
---------------------------
Name: EK200P46.zip
Size: 1480100408 bytes (1411 MiB)
SHA256: 37AA76E407074D1BE67DC3D6C616C7F9CAF9604D9F2129558793316B9A05FE92

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.