×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109765456, Entry date: 03/20/2019
(0)
Rate

Updates for SIMOCODE ES V13 SP2 (TIA Portal)

  • Entry
  • Associated product(s)
Available downloads: Overview of the current and earlier versions

Current version:

Status March 2019: Update 1

This update is valid for the following product:

  • SIMOCODE ES V13 SP2 (TIA Portal)


In conjunction with PROFINET devices Note the following:
 

Devices connected to an enterprise network or directly to the internet must be appropriately protected against unauthorized access, e.g. by use of firewalls and network segmentation. For more information about industrial security, please visit  http://www.siemens.com/industrialsecurity

Bug-fixing:

  • Stability when working with the TIA Portal has been improved, based on the customer feedback.

Installation instructions:

  • The update can only be installed if SIMOCODE ES V13 SP2 (TIA Portal) is already installed (109746269)

  • After each installation of SIMOCODE ES V13 SP2 (TIA Portal), the latest update needs to be installed again.   

Download:


 Registrierung notwendig  SIMOCODE_ES_V13_SP2_Upd1.exe (52,7 MB) 

SHA-256 checksum:   Registrierung notwendig  Code_SIMOCODE_ES_V13_SP2_Upd1.txt (1 KB)
Information about SHA-256:  109483101

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.