×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109765923, Entry date: 04/16/2019
(0)
Rate

Support of multiple passive connections per port by communication processors of S7-1500 and ET 200SP

  • Entry
  • Associated product(s)
Contrary to the information in the function description and in the interoperability list no guarantee can be given for the "Multiport" function for all modules.

Contrary to the information in the function description and in the interoperability list no guarantee can be given for the "Multiport" function (support of multiple passive connections per port) for the following modules. 


 Module Article number
 CM 1542-1 6GK7 542-1AX00-0XE0
 CP 1543-1 6GK7 543-1AX00-0XE0
 CP 1542SP-1 6GK7 542-6UX00-0XE0
 CP 1543SP-1 6GK7 543-6WX00-0XE0


The listed modules only support the function if the property "Support of multiple passive connections per port" is specified with "Yes" in the technical data of the modules.

Alternatively the following solutions are available:

  • Use of different port numbers (2404 and 2405, for example).
  • Use of the active instead of passive established connection.
  • Distribution of the passive connections to multiple CM/CP modules.
  • Use of the local PLC interface(s), because the PLC support the "Multiport" function.




Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit