×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109765925, Entry date: 04/16/2019
(0)
Rate

Utilization of SIPLUS RIC in the (current) TIA Portal

  • Entry
  • Associated product(s)
You can also use SIPLUS RIC in the newer TIA Portal versions.

SIPLUS RIC is currently available in the following versions for utilization in the TIA Portal:

SIPLUS RIC V1.6
This version is available for the product families ET 200, S7-300, S7-400 in TIA Portal V13 SP1.

SIPLUS RIC V1.6 Update 4
This version is available for the product families ET 200SP (incl. Open Controller) and S7-1500 in TIA Portal V13 SP1 and TIA Portal V14.

The use of SIPLUS RIC in TIA Portal V14 SP1 and higher
You can also use SIPLUS RIC in more recent versions of TIA Portal. In each case you open the latest version of the library or the sample project and follow the instructions for upgrading.

If you receive the error message "Library version conflict for...", you will find a solution in the following FAQ:
109765926

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit