×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109766390, Entry date: 04/10/2019
(1)
Rate

Process Historian 2014 SP3 Upd3 and Information Server 2014 SP3 Upd3

  • Entry
  • Associated product(s)
Update 3 is available for Process Historian 2014 SP3 and Information Server 2014 SP3.

What is new?
Update 3 for Process Historian 2014 SP3 and Information Server 2014 SP3 improves the behavior in several areas. For detailed information see the readme file.
  
Installation requirements
The installation of Update 3 for Process Historian 2014 SP3 and Information Server 2014 SP3 requires at least the installation of the following software:    

  • Process Historian 2014 SP3
  • Inforrmation Server 2014 SP3

The Process Historian and Information Server updates are cumulative and include the previous updates. The setup of Update 3 checks which Process Historian and Information Server components are installed on the target computer and updates them.

Readme files
Prior to installation read the notes and compatibility information in the readme files.
 Registrierung notwendig IS_PH_2014_SP3_Upd3_Readme.zip (662,6 KB) 
  
Installation file
The following ZIP file includes the installation file.
 Registrierung notwendig IS_PH_2014_SP3_Upd3.zip (179,9 MB) 

SHA256 Hash Code: 179F1AF36FE814051A9F03380D05AD6912C5E15E15D430536D6CDC1C7382732F
Information on SHA256

Note
Process Historian and Information Server can be used with SIMATIC PCS 7 and SIMATIC WinCC.
To keep your plant permanently up to date, refer to the information in the Compatibility Tool www.siemens.com/kompatool