×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109766528, Entry date: 04/09/2019
(0)
Rate

 Elimination of yellow inspection stickers on SCALANCE modules

  • Entry
  • Associated product(s)
 Elimination of yellow inspection stickers on SCALANCE modules

1. Description 

Because production in Karlsruhe is switching to a digital traceability system in June 2019, the yellow inspection sticker on the SCALANCE modules (new parts and spare parts) will be eliminated.


 


 

 

Each device that was tested and approved will be stored in the traceability database with a serial number.

Only when all production steps are complete and all test results are stored as passed in the database, will the packaging label be printed and the device signed out for shipping.

 


 


 

As of 01.06.2019, the following products/product families will be delivered without inspection sticker:

 

SCALANCE CSM 377/1277/LOGO

SCALANCE M-800

SCALANCE TAP104

SCALANCE S-600

SCALANCE SC-600

SCALANCE W-1700

SCALANCE W-700

SCALANCE X005 / X101

SCALANCE X-100

SCALANCE X-200RNA

SCALANCE X-200/X-200IRT/X-200PRO

SCALANCE X-300/300EEC

SCALANCE XB-000

SCALANCE XB-100

SCALANCE XB-200

SCALANCE XC-100

SCALANCE XC-200

SCALANCE XF-200/XF-200IRT

SCALANCE XF-200BA/XF-200BA IRT/XF-200BA DNA

SCALANCE XP-200

SCALANCE XM-400 incl. port extender

SCALANCE XR-100WG

SCALANCE XR-300WG

SCALANCE XR-300/XR-300EEC incl. media modules

SCALANCE XR-500 incl. media modules

C-PLUG / KEY-PLUG

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.