×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109766533, Entry date: 04/09/2019
(0)
Rate

Firmware update V6.2.2 for SCALANCE XR-500

  • Entry
  • Associated product(s)
Firmware V6.2.2 is hereby available to download for SCALANCE XR-500.

The following features were added:

  • Disabling ring, standby and MRP interconnection ports using WBM and CLI
    It is now possible to disable ring, standby and MRP interconnection ports using WBM and CLI.
  • Extension of the System->Restart function
    Using the "Scheduled Restart" function, you can plan a device restart after expiration of a configurable delay time. This function is available using WBM and CLI.

 

Corrections were made in the following areas:

  • Corrections in the area of PIM Multicast routing
    This firmware update should be used if IP Multicast routing with mobile IP Multicast senders and/or receivers is used or if these are rearranged during operation.

  • Corrections in the area of OSPF routing
    The packets of individual terminal devices were discarded in some cases when OSPF was used as the routing protocol. This behavior has been corrected with this firmware update. The firmware update should therefore be used when using OSPF.

  • Correction of the behavior of the HRP standby slave
    A restart of the HRP standby slave, especially while using the loop detection function at the same time, can create a network loop in some cases.
    We therefore recommend using this firmware update when HRP standby is used.

  • Correction of the link recognition of 10 Gbps SFPs for XR526
    The link recognition of 10 Gbps SFPs when restarting the device has been improved. We recommend using this firmware upgrade when 10 Gbps SFPs are used in the SCALANCE XR526.

 

Firmware V6.2.2 has been released for upgrading the following product variants:  

SCALANCE XR552-12M

6GK5 552-0AA00-2AR2

SCALANCE XR552-12M

6GK5 552-0AR00-2AR2

SCALANCE XR552-12M
(cable outlet at rear)

6GK5 552-0AA00-2HR2

SCALANCE XR552-12M
(cable outlet at rear)

6GK5 552-0AR00-2HR2

SCALANCE XR528-6M

6GK5 528-0AA00-2AR2

SCALANCE XR528-6M

6GK5 528-0AR00-2AR2

SCALANCE XR528-6M
(cable outlet at rear)

6GK5 528-0AA00-2HR2

SCALANCE XR528-6M
(cable outlet at rear)

6GK5 528-0AR00-2HR2

SCALANCE XR526-8C

6GK5 526-8GS00-2AR2

SCALANCE XR526-8C

6GK5 526-8GR00-2AR2

SCALANCE XR526-8C

6GK5 526-8GS00-3AR2

SCALANCE XR526-8C

6GK5 526-8GR00-3AR2

SCALANCE XR526-8C

6GK5 526-8GS00-4AR2

SCALANCE XR526-8C

6GK5 526-8GR00-4AR2

SCALANCE XR524-8C

6GK5 524-8GS00-2AR2

SCALANCE XR524-8C

6GK5 524-8GR00-2AR2

SCALANCE XR524-8C

6GK5 524-8GS00-3AR2

SCALANCE XR524-8C

6GK5 524-8GR00-3AR2

SCALANCE XR524-8C

6GK5 524-8GS00-4AR2

SCALANCE XR524-8C

6GK5 524-8GR00-4AR2

 

 

Third-party software – license conditions and copyright information

You can find the copyright information for the third-party software contained in this product, particularly open source software, as well as applicable license conditions of such third-party software in the ReadMe_OSS file.

Special note for resellers

The information and the license conditions in the Readme_OSS file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.
  Registrierung notwendig  Readme_OSS.htm (20.4 KB)

 

Please read the notes on installation in the product documentation.

You can download the file here.

 Registrierung notwendig  firmware_xr500_xm400_V6p2p2.zip (38.0 MB) 

You can download the gsdml here.

 Registrierung notwendig  gsdml_SCALANCE_XR500_V6p2p2.zip (38.2 KB) 

Hash: "  Registrierung notwendig  gsdml_SCALANCE_XR500_V6p2p2.txt (1 KB)

You can download the private mib here.

 Registrierung notwendig  scalance_x_msps_xr500_V6p2p2.zip (251.0 KB) 

Hash:  Registrierung notwendig  scalance_x_msps_xr500_V6p2p2.txt (1 KB) 

  

 Registrierung notwendig  Liesmich.htm (103.2 KB) 

 Registrierung notwendig  Readme.htm (98.5 KB)

Since changes may be made at short notice, you can find the current version of the readme file with the following link:  109745164

 

Contact for technical issues: Customer Support, DI CS SD CCC TS, Contact form

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.