×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109766534, Entry date: 04/09/2019
(1)
Rate

Firmware update V6.2.2 for SCALANCE XM-400

  • Entry
  • Associated product(s)
Firmware V6.2.2 is hereby available to download for SCALANCE XM-400.

The following features were added:

  • Disabling ring, standby and MRP interconnection ports using WBM and CLI
    It is now possible to disable ring, standby and MRP interconnection ports using WBM and CLI.

  • Extension of the System->Restart function
    Using the "Scheduled Restart" function, you can plan a device restart after expiration of a configurable delay time. This function is available using WBM and CLI.

 

Corrections were made in the following areas:

  • Corrections in the area of PIM Multicast routing
    This firmware update should be used if IP Multicast routing with mobile IP Multicast senders and/or receivers is used or if these are rearranged during operation.

  • Corrections in the area of OSPF routing
    The packets of individual terminal devices were discarded in some cases when OSPF was used as the routing protocol. This behavior has been corrected with this firmware update. The firmware update should therefore be used when using OSPF.

  • Correction of the behavior of the HRP standby slave
    A restart of the HRP standby slave, especially while using the loop detection function at the same time, can create a network loop in some cases.
    We therefore recommend using this firmware update when HRP standby is used.

Firmware V6.2.2 has been released for upgrading the following product variants:  

SCALANCE XM416-4C

6GK5416-4GS00-2AM2

SCALANCE XM408-8C

6GK5408-8GS00-2AM2

SCALANCE XM408-4C

6GK5408-4GP00-2AM2

SCALANCE XM416-4C L3

6GK5416-4GR00-2AM2

SCALANCE XM408-8C L3

6GK5408-8GR00-2AM2

SCALANCE XM408-4C L3

6GK5408-4GQ00-2AM2

 

 

Third-party software – license conditions and copyright information

You can find the copyright information for the third-party software contained in this product, particularly open source software, as well as applicable license conditions of such third-party software in the ReadMe_OSS file.

Special note for resellers

The information and the license conditions in the Readme_OSS file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.
  Registrierung notwendig  Readme_OSS.htm (20.4 KB)

 

Please read the notes on installation in the product documentation.

You can download the file here.

 Registrierung notwendig  firmware_SCALANCE_XM-400_V6p2p2.zip (38.0 MB) 

You can download the gsdml here.

 Registrierung notwendig  gsdml_SCALANCE_XR400_V6p2p2.zip (38.2 KB) 

Hash:  Registrierung notwendig  gsdml_SCALANCE_XR400_V6p2p2.txt (1 KB)

You can download the private mib here.

 Registrierung notwendig  scalance_x_msps_xr400_V6p2p2.zip (492.0 KB) 

Hash:  Registrierung notwendig  scalance_x_msps_xr400_V6p2p2.txt (1 KB)


 Registrierung notwendig  Liesmich.htm (103.2 KB) 

 Registrierung notwendig  Readme.htm (98.5 KB)

Since changes may be made at short notice, you can find the current version of the readme file with the following link: 109745164

 

Contact for technical issues: Customer Support, DI CS SD CCC TS, Contact form

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.