×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109766855, Entry date: 04/17/2019
(0)
Rate

Update of the SIMATIC IPC Image & Partition Creator V3.5 (Software) and new delivery type on USB Flash Drive

  • Entry
  • Associated product(s)
With immediate effect, a new version of the SIMATIC IPC Image & Partition Creator V3.5 (V3.5.4) is supplied on USB Flash Drive. Please note the information regarding the new article number provided at the end of this entry.

This version replaces all previous V3.5 versions.

Due to the new delivery type on a bootable USB 3.0 Flash Drive, a DVD drive is no longer required.
Existing special IPC features such as the creation of an “end customer USB Flash Drive“ remain unchanged.
General information on the SIMATIC IPC Image & Partition Creator V3.5 is provided in the entry 109740914

The support for the new SIMATIC IPCs has been newly integrated in Version 3.5.4:

  • SIMATIC IPC127E
  • SIMATIC IPC647E / IPC847E
  • SIMATIC IPC627E / IPC677E


Note:

The SIMATIC IPC Image & Partition Creator V3.5 on USB Flash Drive will also replace the SIMATIC IPC Service USB Flash Drive 6ES7648-6XA11-0YA0 as per January 1, 2020.

The corresponding product information is scheduled to be issued in May 2019.


Ordering data

Please note:

Due to the new delivery type, a new article number will be assigned to the SIMATIC IPC Image Partition Creator.


With immediate effect, old versions (V3.5) on DVD with the article number 6ES7648-6AA03-5YA0 are no longer available.

Product designation

Article number

Start of delivery

SIMATIC IPC Image & Partition Creator V3.5,
2 languages (DE / EN), USB Flash Drive

6ES7648-6AA13-5YA0

04/2019

 

License conditions

With each license, the SIMATIC IPC Image & Partition Creator V3.5 may be installed or run without installation on only one device.


  




Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.