×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109767181, Entry date: 05/07/2019
(0)
Rate

Hardware Support Package “HSP 0295 SIMOCODE pro V EIP / pro V”

  • Entry
  • Associated product(s)
The Hardware Support Package “HSP0295 SIMOCODE pro V EIP V1.1 / pro V V4.1“ for STEP 7 V15.1 and SIMOCODE ES V15.1 is available for download.

By installing the HSP0295, the hardware catalog of STEP 7 V15.1 and SIMOCODE ES V15.1 can be updated with the following SIMOCODE pro firmware versions:

  • SIMOCODE pro V (PROFIBUS) basic unit firmware V4.1

  • SIMOCODE pro V EIP (EtherNet/IP) basic unit firmware V1.1

Requirement

The HSP0295 requires the following installation:

  • STEP 7 V15.1 or SIMOCODE ES V15.1

  • The “HSP_V15_1_0295_001_SIMOCODE_SMC3_R3.isp15_1” file must be available on the PC.

Installing HSP in the TIA Portal

  1. Open the TIA Portal with administrator rights.
  2. Select "Options > Support Packages" from the menu. The "Additional information > Installation of Support Packages" dialog box opens.
  3. Click the "Add from file system" button.
  4. Select the directory of the “HSP_V15_1_0295_001_SIMOCODE_SMC3_R3.isp15_1” file in the file system.
  5. Click "Open". The file is added in the TIA Portal.
  6. Activate the “HSP0295 SIMOCODE pro V EIP / pro V" in the “Additional information” dialog.
  7. Click the "Install" button. A dialog box opens.
  8. Click "Next". Installation starts.

Result

After successful installation, the "Detailed information" dialog shows the "HSP0295 SIMOCODE pro V EIP / pro V" as installed.

Download

 Registrierung notwendig  HSP_V15_1_0295_001_SIMOCODE_SMC3_R3.zip (1,8 MB)

SHA-256 Prüfsumme:  Registrierung notwendig  Code_HSP_V15_1_0295_001_SIMOCODE_SMC3_R3.txt (1 KB)

Information zu SHA-256: 109483101

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.