×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109767410, Entry date: 05/13/2019
(51)
Rate

Information and Content LOGO! Soft Comfort V8.2 SP1

  • Entry
  • Associated product(s)
New firmware V1.82.01, LOGO! Soft Comfort V8.2 SP1 and LOGO! Web-Editor V1.01 as download available.

The V8.2 SP1 update is designed for the following products


Products

Update information

LOGO! 8.2, all basic modules

Update from FW V1.82.01 to V1.82.02

LOGO! Soft Comfort 8.2

Update from V8.2 to V8.2 SP1

LOGO! Web Editor (LWE)

Update from V1.0 to V1.0.1


The V8.2 SP1 update includes the following improvements/changes


All LOGO! 8.2 basic devices

 

Security vulnerability fix for 774850

All LOGO! basic modules and LOGO! Soft Comfort

Threshold trigger now also supports inputs I3 to I6 on basic devices without fast counters

All LOGO! basic devices without fast counters

LOGO! Soft Comfort

 

Support of LOGO! BM firmware V1.82.02

LOGO! Soft Comfort Update from V8.2 to V8.2.1

Improved representation und presentation in portrait format

LOGO! Soft Comfort Update from V8.2 to V8.2.1

Improved simulation in LAD editor

LOGO! Soft Comfort Update from V8.2 to V8.2.1

Copy & paste in LAD editor

LOGO! Soft Comfort Update from V8.2 to V8.2.1

Improved presentation when sorting I/O names

LOGO! Soft Comfort Update from V8.2 to V8.2.1

LOGO! Web Editor

 

Improved representation of assigned images for pages in German with a high resolution

LOGO! Web Editor update from V1.0 to V1.0.1


Devices affected

         

Designation / Name

 Article No. / Order number

LOGO! 230 RCE

6ED1052-1FB08-0BA0

LOGO! 24RCE

6ED1052-1HB08-0BA0

LOGO! 230RCEo

6ED1052-2FB08-0BA0

LOGO! 24RCEo

6ED1052-2HB08-0BA0

LOGO! 12/24RCE

6ED1052-1MD08-0BA0

LOGO! 12/24RCEo

6ED1052-2MD08-0BA0

LOGO! 24CE

6ED1052-1CC08-0BA0

LOGO! 24CEo

6ED1052-2CC08-0BA0

LOGO! Soft Comfort V8.2

6ED1058-0BA08-0YA1

LOGO! Web Editor V1.0

Without (component of LOGO! Soft Comfort)

            

Note:
The firmware update described in this article can only be carried out in devices named in the list of affected devices. 
 

Procedure for firmware update of basic devices


Ensure that the power supply of the LOGO! basic device remains stable throughout the entire firmware update and within the range described in the manual.

The firmware update can only be carried out in LOGO! 8 basic devices with order number 6ED1052-xyy08-0BA0 and firmware version V1.82.01.

Identification of LOGO! 8 versions:

  1. The FW version can be read out on the LOGO! 8 display, or with LOGO! Soft Comfort
  2. The order number also appears on the front of the basic device.


Link to the Download LOGO! Soft Comfort V8.2 SP1

The files required for the update as well as instructions for carrying out the firmware update can be found here:
link to FW update:  109767413

We recommend that all users perform the firmware update describe above for the devices listed in the table.


Procedure for updating LOGO! Soft Comfort

  1. Load the necessary data for your PC operating system from the LOGO! website
  2. Start the installation as Admin


Procedure for updating the LOGO! Web Editor (LWE)

  1. Download the necessary data from the LOGO! website
  2. Back up your existing LWE projects
  3. Uninstall LOGO! Web Editor V1.0
  4. Start the installation of the LOGO! Web Editor V1.01 as Admin


SHA-256 checksum:

A check to see whether a file has been changed during transmission or by third parties can be performed with a SHA-256 checksum comparison. The file integrity (no change) is assured if the SHA-256 checksum you calculated and the Siemens checksum are identical. 
You can find the SHA-256 checksum provided by Siemens in the respective file download.
Instructions on how to determine the SHA256 checksum of a file are available here:
https://support.industry.siemens.com/cs/ww/en/view/109483101


Security information

Siemens provides products and solutions with industrial security functions that support the secure operation of plants, systems, machines and networks.
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept.

Customers are responsible for preventing unauthorized access to their plants, systems, machines and networks. Such systems, machines and components should only be connected to an enterprise network or the internet if and to the extent such a connection is necessary and only when appropriate security measures (e.g. firewalls and/or network segmentation) are in place.

For additional information on industrial security measures that may be implemented, please visit  https://www.siemens.com/industrialsecurity

Siemens’ products and solutions undergo continuous development to make them more secure. Siemens strongly recommends that product updates are applied as soon as they are available and that the latest product versions are used. Use of product versions that are no longer supported, and failure to apply the latest updates may increase customer’s exposure to cyber threats.

To stay informed about product updates, subscribe to the Siemens Industrial Security RSS Feed under https://www.siemens.com/industrialsecurity


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.