×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109767809, Entry date: 06/05/2019
(0)
Rate

Conversion of S7-1500 / ET 200MP modules for use in installation altitudes above 2000 m

  • Entry
  • Associated product(s)
With immediate effect, most of the S7-1500 modules are available for use in altitudes above 2000 m.

This function extension allows the use of SIMATIC S7-1500 in industrial or infrastructure plants installed at very high altitudes, such as, for example, in South America.

Typical applications include, for example, ropeways, wind power plants, tunnels, automotive plants or mines.

Please note that the entire range of products will be migrated successively.

List of currently migrated modules:

A current list of S7-1500 modules which can be operated at altitudes above 2000 m is included in the
"Product information for S7-1500: Use of (F-)CPUs at heights > 2000 m": 109763260

Note:

The maximum permissible installation altitude depends on the relevant module.

Please also read the information provided in the manual respectively the product information. 
"Product information for the S7-1500/ET 200MP documentation": 68052815


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.