×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109767874, Entry date: 05/22/2019
(0)
Rate

N53x-1DBx1 - FW status is not displayed correctly in ETS

  • Entry
  • Associated product(s)

Problem:

The current firmware version of the N53x is required, but under Device Info in the ETS the correct information is not displayed.

 

Hint:

FW 03 is always displayed under Device info in ETS5, independent of FW installed in the device. The Firmware Download Tool provides the solution.

 

Solution:

The Firmware Download Tool is required to read the currently installed firmware version from the switching actuator. This can be found on our www.siemens.de/gamma-fdt page.

After installation open the tool, please note that only Siemens interfaces are compatible. After opening the tool, select an interface, switch the switching actuator to programming mode and search. Then you can read out the currently installed firmware version under Details. At the same time, the tool also shows whether an update is available, if available, please execute.

Example:

FW V01            ->         00 1a

FW V02            ->         00 02

FW V03            ->         00 13








Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.