×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109768094, Entry date: 07/12/2019
(0)
Rate

User calibration of SIMATIC analog modules

  • Entry
  • Associated product(s)
The application example describes the steps for calibration of analog modules via SIMATIC HMI devices.

The user calibration is controlled by the data sets (DS). The example describes the method to use data sets. The library provides a function block for S7-CPUs and a template for SIMATIC HMI devices to implement the function in the user program.

Figure 1 shows the steps required for the user calibration of an instruction to the analog module.


Figure 1

The SIMATIC HMI device shows the calibration values read from the analog module.


Figure 2

Documentation and Project
  Documentation (2,4 MB)
 Registrierung notwendig  Library for STEP 7 V15.1 (6,6 MB)
 Registrierung notwendig  Project for STEP 7 V15.1 (29,3 MB)


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.