×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109768712, Entry date: 07/04/2019
(6)
Rate

Why does STEP 7 (TIA Portal) V15.1 crash when you are looking for cross-references with the S7-1200 CPU?

  • Entry
  • Associated product(s)
The behavior occurs with STEP 7 (TIA Portal) V15.1 Update 2 and is cleared with Update 3. Install the Update 3 to your STEP 7 (TIA Portal) V15.1.

Description
The download of Update 3 for STEP 7 (TIA Portal) V15.1 you will find in the TIA Portal information system, by
Updates for STEP 7 V15.1 and WinCC V15.1

Consider the following informations so long as you work with STEP 7 (TIA Portal) V15.1 Update 2.

With STEP 7 (TIA Portal) V15.1 Update 2 it might happen that when you open the Cross-reference Editor, STEP 7 (TIA Portal) crashes if you are using the timer types TON, TOF, TP or TONR. You also get the error message shown in Fig. 1.
 


Fig. 1

If you click on the "Show data" button, you get the information from the TIA Portal Diagnostics Report.
 


Fig. 2

However, the program crash only happens when the block is used in a CPU of the S7-1200 product family. If you copy the same block into the program folder of a S7-1500 CPU (in the same project), the cross-reference search does not cause a crash.

​The behavior described above is cleared with Update 3 for STEP 7 (TIA Portal) V15.1. With the Newsletter, you can be informed when the download for Update 3 (planned for August 2019) will be available to you. 

Remedy
For the time being use the menu command "Edit > Search in project".
 


Fig. 3

Note
If the menu command "Search in project" is grayed out, you have to enable "Global Search" beforehand. In STEP 7 (TIA Portal) V15.1 you open the dialog "Options > Settings" and then navigate to "General > Search in project". Enable the function "Enable 'Search in project'".
 


Fig. 4

Additional Keywords
Crash



Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.