×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109769093, Entry date: 06/07/2021
(6)
Rate

S7-1500R/H AddIn

  • Entry
  • Associated product(s)
To connect a PROFINET device to a redundant system S7-1500R/H/HF, it is necessary to set the correct watchdog time for each device. The S7-1500R/H Add-In, as a context menu function for each PN IO device connected to an R/H/HF system, calculates the correct factor and updates it in the settings.

The S7-1500R/H Add-In expands the shortcut menu of the project tree in the TIA Portal and facilitates the automatic configuration of the watchdog factor on PN IO devices of the selected R/H/HF systems, either as a simple progress dialog or as a list display.




Documentation and Addin file

  Documentation (684,2 KB)
 Registrierung notwendig  AddIn file for TIA Portal V17 (51,1 KB)
 Registrierung notwendig  AddIn file for TIA Portal V16 (45,0 KB)

Link to TIA Portal Add Ins
109773999

Last Changes
Release of the Add-In of TIA Portal V17

Additional Keywords
sup_applications


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.