×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109770113, Entry date: 08/08/2019
(0)
Rate

SICAM A8000 CP-8050 Package V0320

  • Entry
  • Associated product(s)
Release Package V0320 Firmware für SICAM A8000 CP-8050

Firmware update for

  • 6MF28050AA00, CP-8050 Master Modul

Previous version

SICAM A8000 CP-8050 Package V03 Update


Installation Notes

The update of the firmware and (if necessary) of the associated adaption of the configuration can be performed with the SICAM TOOLBOX II or with SICAM WEB. The loading of the firmware is also possible without a tool, solely via the SD card.

Required user action via SICAM Device Manager:

The firmware files with the extensions * .bin and * .web, from the unzipped file BinaryUpdate.zip, can be stored on any PC directory and are imported into the target system via the menu item "Load firmware" in the SICAM Device Manager.
Only digitally signed firmwares are supported.

Required user action via SICAM TOOLBOX II:

To be able to perform an update, first the new firmware must be imported into the SICAM TOOLBOX II (firmware files from the unzipped file TBIIUpdate.zip). For the adaption of the configuration in the target device the settings must be upgraded in the OPM II (system technique), afterwards the firmware must be loaded into the target device.

Required user action via SICAM WEB:

The update of the firmware can be performed via the corresponding menu “Firmware update“. (Firmware files from the unzipped file BinaryUpdate.zip)

Required user action with SD card:

First the SD card must be removed from the target device, then the new firmware  (firmware files from the unzipped file BinaryUpdate.zip) can be copied into the directory “IN” of the SD card. Afterwards the SD card must be put into the target device, that thereupon performs a startup.


Releasenotes

 Registrierung notwendig  ReleaseNotes.zip (133,2 KB)


SICAM WEB Update

 Download unterliegt Exportcontrolle  SWEBUpdate.zip (46,0 MB)


SICAM TOOLBOX II Update

 Download unterliegt Exportcontrolle  TBIIUpdate.zip (49,9 MB)


Package Content


103MI0 Protection Master IEC60870-5-103 Version: 03
TBII Update: 85502603.
SWEB Update: 103MI003.F


AGPMI0 AGP Master (Ankopplung der Abzweiggebundenen Prüfeinrichtung) Version: 03
TBII Update: 85712603.
SWEB Update: AGPMI003.F


BPPI0 Point-Point Traffic IEC60870-5-101 Version: 03
TBII Update: 85512603.
SWEB Update: BPPI003.F


CPCI85 Central Processing/Communication Version: 0320 **NEW**
TBII Update: 80852403.20
SWEB Update: CPCI8503.F20


DNPiI1 DNP3 TCP/IP Slave Version: 03
TBII Update: 85632603.
SWEB Update: DNPII103.F


DNPSI0 DNP3 Slave Version: 03
TBII Update: 85622603.
SWEB Update: DNPSI003.F


DPMI0 PROFIBUS-DP Master + ext. netHOST Version: 03
TBII Update: 85652603.
SWEB Update: DPMI003.F


DSFGI0 DSFG-Bus Slave (instance+cross traffic) Version: 03 **NEW**
TBII Update: 85722603.
SWEB Update: DSFGI003.F


EPCI85 Extended Processing/Communication Version: 0310
TBII Update: 80872903.10
SWEB Update: EPCI8503.F10


ETI4 Ethernet Interface IEC60870-5-104 Version: 0310 **NEW**
TBII Update: 85202603.10
SWEB Update: ETI403.F10


ETI5 Ethernet Int. 1x100TX IEC61850 Ed.2 Version: 0311
TBII Update: 85212603.11
SWEB Update: ETI503.F11


FWI4 IEC60870-5-104 HW based FW Version: 0310
TBII Update: 85702603.10
SWEB Update: FWI403.F10


IOMI65 Universal Signal In-/Output SICAM TM I/O Module Version: 0310
TBII Update: 85312203.10
SWEB Update: IOMI6503.F10


IOMI85 Universal Signal In-/Output SICAM I/O Module Version: 0310
TBII Update: 85302203.10
SWEB Update: IOMI8503.F10


MBCiI0 MODBUS TCP/IP Master (Client) Version: 03
TBII Update: 85592603.
SWEB Update: MBCII003.F


MBSiI0 MODBUS TCP/IP Slave (Server) Version: 03
TBII Update: 85602603.
SWEB Update: MBSII003.F


MODMI0 MODBUS Master Version: 03
TBII Update: 85572603.
SWEB Update: MODMI003.F


MODSI0 MODBUS Slave Version: 03
TBII Update: 85582603.
SWEB Update: MODSI003.F


OPUPI0 AMQP/MQTT (IOT) Version: 0301 **NEW**
TBII Update: 85682603.01
SWEB Update: OPUPI003.F01


OPUPI1 Mindsphere (IOT) Version: 01
TBII Update: 85672601.
SWEB Update: OPUPI101.F


PNMI0 PROFINET I/O Master + ext. netHOST Version: 03
TBII Update: 85662603.
SWEB Update: PNMI003.F


SWEB00 SICAM WEB Version: 0511
SWEB Update: SWEB0005.F11


U80ZI0 EAW URSATRON U8000 Master Version: 03 **NEW**
TBII Update: 85732603.
SWEB Update: U80ZI003.F


UMPMI0 Multipoint Master IEC60870-5-101 Version: 03
TBII Update: 85532603.
SWEB Update: UMPMI003.F


UMPSI0 Multipoint Slave IEC60870-5-101 Version: 03
TBII Update: 85542603.
SWEB Update: UMPSI003.F


VLZI0 ÖBB VLZ (PIPS1 protocol) EE Version: 01
TBII Update: 85692601.
SWEB Update: VLZI001.F

Terms of Use

Reservation regarding future software downloads

Die hier zum Download angebotene Software wird derzeit unentgeltlich zur Verfügung gestellt. Siemens behält sich vor, die Software zukünftig gegen Entgelt zur Verfügung zu stellen.

General License Conditions

 Registrierung notwendig  EM_DG_General_License_Conditions_Software_10_2015.pdf (142,4 KB)

Third Party Software - Terms of License and Copyright

Open Source Software:
Among other things, this product contains Open Source Software that was developed by third parties. The Open Source Software included with this product and the relevant Open Source Software license agreement can be found in Readme_OSS. The Open Source Software program is protected by copyright. You are permitted to use the Open Source Software according to the Open Source Software license agreement.
You can download the Readme_OSS file here:

 Registrierung notwendig  ReadmeOSS.zip (746,5 KB)

Special Information for Resellers

The information and the license terms in the Readme_OSS file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

Disclaimer regarding use of previous software versions

Siemens’ products and solutions undergo continuous development to remain leading in many fields of technology and to represent the state of the art. Siemens strongly recommends to apply product updates as soon as available and to always use the latest product versions.

Use of product versions that are no longer supported, and failure to apply latest updates may increase customer’s exposure to system degradation. By downloading unsupported product version the customer confirms that he operates this outdated product version at his own risk and responsibility and with full awareness of potential risks and consequences and confirms his conscious decision to abandon the enhancements available only with the current version as listed in [1]. The customer has read that he should actively plan the upgrade of his installed base to the latest supported product versions.

The Customer hereby explicitly agrees and accepts that Siemens does not cover any warranty or liability, explicitly or implicitly, regardless of any legal reason, for any damages or losses caused directly or indirectly by the use of outdated/unsupported product versions.
The Customer shall indemnify and hold Siemens harmless against any third-party claims existing or arising in this connection.

[1] Further information about Siemens ProductCERT and Siemens CERT


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.