×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109771049, Entry date: 06/03/2020
(1)
Rate

The SINAMICS G120X Firmware V1.03.00

  • Entry
  • Associated product(s)
With the immediately effect the SINAMICS G120X firmware version V1.03.00 is released for download.

1. Scope

The new SINAMICS G120X firmware version V 1.03.00, which is the succesor of the SINAMICS G120X firmware version V 1.02.00,  is offered as firmware download.

All the SINAMICS G120X frame sizes of the following hardware variants are supported by the SINAMICS G120X firmware version.

 V 1.00.01  V 1.01.00 V1.02.00 V1.03.00
 SINAMICS G120X PN 400V
Yes
 Yes  Yes Yes 
 SINAMICS G120X PN 690V  Yes Yes YesYes
 SINAMICS G120X DP 400V  No Yes  Yes Yes 
 SINAMICS G120X DP 690V  No Yes  YesYes 
 SINAMICS G120X USS 400V  No Yes  YesYes
 SINAMICS G120X USS 690V  No Yes  YesYes
 SINAMICS G120X PN 200V   No  Yes   Yes Yes
 SINAMICS G120X DP 200V   No  Yes   YesYes
 SINAMICS G120X USS 200V  No Yes   YesYes


The SINAMICS G120X hardware variants information can be found from 109762168.


The following engineering systems are offered for configuring the SINAMICS G120X firmware version V 1.03.00 (NEW!!!)

 Engineering system Product Information 
 IOP-2 V2.6Available in September 2020
 G120 SMART Access V01.05Available in November 2020
 BOP-2Support included from SINAMICS G120 V4.7 SP10 


The following engineering systems are offered for configuring the SINAMICS G120X firmware version V 1.02.00

 Engineering systemProduct information  
 IOP-2 V2.5 HF1109762019
 G120 SMART Access V01.03.02109780981
 BOP-2 Support included from SINAMICS G120 V4.7 SP10


The following engineering systems are offered for configuring the SINAMICS G120X firmware version V 1.01.00.

 Engineering systemProduct information  
 IOP-2 V2.4.x 109762019 
 G120 SMART Access V01.03.01 109769429 
 BOP-2 Support included from SINAMICS G120 V4.7 SP10

2. Function description

The SINAMICS G120X firmware provides rich functions for pump and fan applications. An overview of these functions is presented in Figure 1.



Figure 1 The SINAMICS G120X firmware functions overview

The detailed descripition of each firmware functions can be found from the SINAMICS G120X  Registrierung notwendig  SINAMICS-G120X--Firmware_Functions.pptx (6,1 MB) 

The new SINAMICS G120X firmware version V 1.03.00 provides additional functions in addition to the SINAMICS G120X firmware version V 1.02.00 (NEW!)

 FunctionDescription 
Free Function Blocks (FFB)

•Integrated 16 different FFB types and 40 FFBs.

•Including logical, arithmetic, timer, memory, switch, control FFBs

•Only for FSA to FSG 


The new SINAMICS G120X firmware version V 1.02.00 provides additional functions in addition to the SINAMICS G120X firmware version V 1.01.00

 FunctionDescription 
 Multi-pump function
•Shorten the time consumption of pump switch-in & -out
•Optimize the cycling mode
•Optimize the logic of service mode
 

Pipe filling

•Add P29609: Able to activate pipe filling function via BI parameter
•P29611 =3: New mode for enabling pipe filling function according to the pressure after servo on.
•R29619: Extended Control Word

Deragging

•P29590=4: New mode for enabling by BI while running.
•R29599: New customer parameter, of which the bit 12 and bit 13 indicate the deragging count state.
•P29605/06/07: New parameters for monitoring configuration
2-/3- wire control function  •Update description of parameter p3330, p3331, p3332,r3333, p3334
•Adjust access level of p3334 from 4 to 3
Parity setting for ModBus  •P2031=3: New parity mode for no parity & 1 Stop bit


The new SINAMICS G120X firmware version V 1.01.00 provides additional functions in addition to the SINAMICS G120X firmware version V 1.00.00.

 FunctionDescription 
 PT100 sensor
  • Supporting PT100 sensor for motor temperature protection
  • Temperature evaluated via a converter analog input
  • Supporting 2-wire and 3-wire connection
 Load monitoiring
  • Optimized default monitoring threshold values for blocking, leakage and dry-running protection
  • Default monitoring threshold values adjusted automatically according to application types 
New macros  
  •  new introduced macos
  •  simplify the commissioning effort for different applications
  •  See the overview of marocs in Figure 2  and Figure 3




Figure 2 Marcos 41 to 47


Figure 3 Marcos 48 to 57

3. Third-party software – license conditions and copyright notes

You can find the copyright notes on the third-party software, especially Open Source Software, as well as applicable license conditions for this type of third-party software in the file READ_OSS.HTM file.

Special note for resellers

The notes and the license conditions contained in the READ_OSS.HTM file must be passed on to the purchaser in order to avoid the reseller and purchaser from violating the licensing conditions.

Availability of the source code

Some license conditions of third-party software components used in this product may oblige us to provide you with the source text and further information for these components. You can find this information either directly on the product itself or with the product (e.g. on a mass storage medium, DVD). Should this not be possible due to technical reasons, Siemens will send you this OSS Source Code against payment of the handling expenses. Please contact the address specified at the end of this section regarding this matter.

Siemens AG 
Digital Factory
Customer Services DF&PD
DF CS SD CCC TS
Gleiwitzer Str. 555
90475 Nuremberg, Germany

Fw v1.03.00  Registrierung notwendig  Read_OSS_v1.03.00.htm (1,5 MB)

FW v1.02.00:  Registrierung notwendig  READ_OSS_v1.02.00.HTM (1,5 MB)

FW  v1.01.00  Registrierung notwendig  ReadMe_OSS.html (1,6 MB)

4. Download

The SINAMICS G120X FW v1.03.00.05 can be downlaoded from here (NEW!!!) Registrierung notwendig  G120X_04712723_OA_1030005_BIOS_04703703.zip (15,6 MB)

The SINAMICS G120X FW v1.02.00.12 can be downlaoded from here:  Registrierung notwendig  G120X_04712795_OA_1020012_BIOS_04703703.zip (15,6 MB) 

The SINAMICS G120X FW V1.01.00.13 can be downloaded from here:  Registrierung notwendig  G120X_BS_04712708_OA_1010013_BIOS_04703703.zip (15,3 MB) 

A memory card is needed in order to upgrade the SINAMICS G120X firmware.

The procedure of preparing the memory card is described as the following:

1. Download the required firmware to your PC from this SIOS Note

2. Extract the files to a directory of your choice on your PC.

3. Transfer the unzipped files into the root directory of the memory card. See an example from Figure 4.




Figure 4  Example of memory card contents after the file transfer

Depending on the firmware, the filenames and the number of files may differ from the display above.

The "USER" directory does not exist on unused memory cards. After the memory card is plugged in for the first time, the converter creates a new "USER" directory.

In terms of further information regarding Firmware upgrade, please refer to the instructions given in the "Firmware upgrade" chapter 10.3 in the Operating instructions of the SINAMICS G120X.

109769350

5. Useful links

The SINAMICS G120X GSDXML and GSD file
109763250

The SINAMICS G120X EDS file
78026217

The SINAMICS G120X FDI Package (PN only)
109766204

Drive ES PCS7 V9.0 SP2 (Classic Style) libraries as support for the SINAMICS G120X 
109769471

Drive ES PCS7 APL V9.0 SP2  libraries as support for the SINAMICS G120X 
109771478

6. List of faults and alarms

The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware. They only include an export of the "Alarm messages" text for the SINAMICS G120X in the "xml" format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, as far as the SINAMICS G120X product is concerned, no additional support can be provided here.

FW v103.00  Registrierung notwendig  FW v1.02.00   Registrierung notwendig  G120X_04712717_1020009_alarm_lists.zip (313,5 KB) 


FW v1.01.00 Registrierung notwendig  G120X_04712708_1010013_alarm_lists.zip (312,4 KB)



Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.