×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109771777, Entry date: 04/17/2020
(7)
Rate

Delivery Release SIMATIC WinCC Unified V16

  • Entry
  • Associated product(s)
Information SIMATIC WinCC Unified: More than an HMI

SIMATIC WinCC Unified V16 is the new visualization system in the TIA Portal.

From machine-level operator control to integration of IT systems in automation, WinCC Unified is not only fit for today's demands but also for the demands of the future.

The system is impressive in its use of native web technologies (HTML5, SVG and JavaScript) as well as its high degree of openness thanks to high-performance interfaces for data exchange.


Key advantages at a glance

Technology
WinCC Unified has been completely redesigned and uses native web technology such as HTML5, SVG and JavaScript. This enables access to visualization from any modern web browser, without the need to install additional plug-ins. Configuration is performed in the proven TIA Portal.




Scalability
WinCC Unified offers a fully scalable scope of functions, from the machine-level application to distributed SCADA systems.
HMI projects or project components can be transferred from a machine-level application to a SCADA application.




Everywhere
Due to its modern architecture, a wide range of functions can be executed by WinCC Unified in various environments. In addition to the classic "on-premise" application cases, it will also be able to run WinCC Unified in an Edge or Cloud environment.
In its initial version, WinCC Unified is available for panel- and PC-based solutions. Its use in the Edge and Cloud environment will be possible with a subsequent delivery stage.




Openness (Integration Platform)
Thanks to the interfaces integrated into the system, WinCC Unified offers a high degree of openness right from the start. 
By providing an open API interface, a WinCC Unified project can be automatically generated via the user's own application.  On the other hand, WinCC Unified features an API interface to enable extensive data exchange with other systems during operation of Unified. A new OpenPipe interface can be used to link external applications with a WinCC Unified.



For more information, also visit the following website: The future of visualization starts now!

SIMATIC WinCC Unified ES V16 - Notes for the engineering software

Note on licensing of engineering software
Every customer who purchases a license for WinCC Comfort V16, WinCC Advanced V16 or WinCC Professional V16, or receives it as part of the Software Update Service (SUS), can use the corresponding WinCC Unified Version free of charge.

License compatibility
A WinCC Unified ES can be installed together with a WinCC Advanced ES on a single computer via the installation. Valid licenses for a WinCC Unified ES can also be used for engineering of a WinCC Advanced (and vice versa).

A WinCC Unified ES cannot be installed parallel to a WinCC Professional ES on only one computer. Valid licenses for a WinCC Unified ES can also be used for engineering of a WinCC Professional (and vice versa). Licenses must be transferred to the WinCC Professional ES computer for this.


Operating systems


Configuration

Remark

Windows 10 Pro

Windows 10 Pro Version 1809
Windows 10 Pro Version 1903

64-bit

Windows 10 Enterprise

Windows 10 Enterprise Version 1809
Windows 10 Enterprise Version 1903

Windows 10 IoT Enterprise 
LTSB (Test for IPC)

Windows 10 IoT Enterprise 2015 LTSB
Windows 10 IoT Enterprise 2016 LTSB
Windows 10 IoT Enterprise 2019 LTSC

Windows Server 2012 R2 StdE
Windows Server 2016 Standard
Windows Server 2019 Standard

Full installation

64-bit


SIMATIC WinCC Unified Runtime V16 - Notes for the runtime software

Important notes
Please read the notes on WinCC Unified Runtime V16:   ReadMe (106.1 KB) 

Also read the entry page on updates of WinCC Unified PC Runtime: 109773716 

Basic functionality
The following functionality is already included with the basic product


 User interface Scalable for all devices
 Connectivity Connects automation and IT via standard interfaces
 Alarming Know what is happening in your plant
 Reporting Plant reports (based on Microsoft Excel); minimum: MS Excel 2016 - Build 16.0.6769 (32-bit or 64-bit)
 Scripting Wide-ranging scripting options of Runtime
 Runtime Openness Extended functionality and integration platform
 Plant hierarchy Modular and standardized machine and plant designs
 User administration Local user administration and access control
 Client access

 Basic version provides licensed access by 2 clients.



Available options

Basic options


File-based loggingLocal data acquisition for small to medium applications
File-based logging is the standard logging variant and is activated by licensing logging tags. Up to 5,000 additional logging tags can be purchased for file-based logging.
The data-based logging option is needed for a higher number of logging tags or if long-term archiving is required; 

Parameter control

Uniform management and control of machine or production parameters

Unified collaboration

Assembling a distributed configuration

Clients

Flexible web-based, remote operation and control;
In addition to the two client licenses already included in the basic system, more access can be purchased in addition.
5 web clients can access a Runtime station simultaneously for non-server Windows operating systems. For more than 5 clients, a Windows Server operating system is required. 

 

SCADA options


Databased storageExtensive, high-performance, long-term archiving
This data-based logging option enables SQL-based logging.
Logging Tags must be purchased in addition for data-based logging. When switching from file-based to data-based logging, Logging Tags already purchased can continue to be used.


Requirements for a Unified Runtime station

Hardware requirements (PC systems)

The hardware equipment essentially determines the performance, especially for larger projects and visualization tasks, a powerful processor and more memory should be selected. Depending on the options used, e.g. Logging, additional free hard disk space is required.

Hardware

Requirements

Processor type

x64 processor, recommended Intel Core i3 or better
for small applications also Intel Atom or Intel Celeron

RAM

4 GB

Free disk space

10 GB, 8GB CF


Operating systems (PC systems)


Configuration

Remark

Windows 10 Pro

Windows 10 Pro Version 1809
Windows 10 Pro Version 1903

64-bit

Windows 10 Enterprise

Windows 10 Enterprise Version 1809
Windows 10 Enterprise Version 1903

Windows 10 IoT Enterprise
LTSB (Test for IPC)

Windows 10 IoT Enterprise 2015 LTSB
Windows 10 IoT Enterprise 2016 LTSB
Windows 10 IoT Enterprise 2019 LTSC
Windows Server 2012 R2 StdE
Windows Server 2016 Standard
Windows Server 2019 Standard

Full installation

64-bit


Windows-specific software settings for IIS (Internet Information Services)

To be able to install WinCC Unified Runtime on a "WinCC Unified Runtime Station", a Microsoft IIS with the following settings must be activated there:

  • HTTP error

  • HTTP redirect

  • Standard document

  • Static content

  • .NET Extensibility 3.5

  • ASP

  • ASP.NET 4.5

  • ISAPI extensions

  • ISAPI filters

  • Compression of dynamic content

  • Compression of static content

  • Request filtering


Additional software requirements
TopicVersion / SettingNote
 Web browserThe browser must support HTML5. 
 User rights for installationAdministrator rights 
 Simatic NET >V13 SP1

You need this license to use Runtime Unified with more than 10 connections.

 

Ports
  • HTTP: 80
  • HTTPS: 443
  • TIA administrator: 8888

Virtualization

  • VMware ESXi 6.5 or higher
  • VMware Workstation 12.5.5 and  VMware Player 12.5.5
  • VMware Workstation 15.0.2 and VMware Player 15.0.2 or higher
  • Microsoft Hyper-V Server 2016  or higher

Antivirus software
  • Symantec Endpoint Protection 14.0
  • McAfee Endpoint Security (ENS) 10.5
  • Trend Micro "Office Scan" 12.0
  • Kaspersky Endpoint Security 11.1
  • Windows Defender (as part of Windows operating systems)
  • Qihoo 360 "Safe Guard 11.5" + "Virus Scanner"

Requirements for a Unified Runtime Client

Operating system (client)

Recommended browser

Microsoft Windows

Google Chrome (preferred)
Mozilla Firefox
Microsoft Edge

Android

Google Chrome (preferred)
Firefox
Edge

iOS, Mac

Safari (preferred)
Google Chrome
Firefox
Microsoft Edge

Ordering data
The products with article numbers (order numbers) are listed in the attached files.
 Registrierung notwendig wincc_unified_v16_productlist.xlsx (27.8 KB)

Compatibility to other SIMATIC products
You can find the compatibility statements on automation and drive technology in the compatibility tool of Industry Online Support. Entry ID 64847781 

Quick link to the compatibility tool
German: http://www.siemens.de/kompatool
English: http://www.siemens.com/kompatool


More information

TIA Portal V16 offers a large variety of new functions for existing products




Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.