×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109772052, Entry date: 10/09/2019
(0)
Rate

SIMATIC MV500 firmware update version 1.2

  • Entry
  • Associated product(s)
The SIMATIC MV500 firmware version 1.2 is available immediately for download free-of-charge.

Firmware version 1.2 is the successor to the firmware version 1.1. The firmware is part of the SIMATIC MV500 product series.

 

The modified functions of firmware versions 1.2 relative version 1.1 are:

  • Auto-setup: Full program
    The use of full program adaptation to programs with specific unusual setting combinations resulted in errors in the display or processing of the adaptation steps.

  • Response time of digital triggers
    When the DI/DO trigger was used, this resulted in a delay with measurable variation (in the microsecond range) between the application of the trigger signal and the triggering of the image acquisition. The response time of the DI/DO trigger has been significantly increased and stabilized.

  • Code type "DotCode"
  • The code type "DotCode" now supports the FNC1 format code of GS1 coding.

  • Web-based management in Chinese
    Access to the camera was only possible from the user interface if the language was set to Chinese.


  • Communication > Use > Connection> Save source program
    This setting was not included in device backups and could therefore not be restored during loading of a data backup (also in the event of a firmware update).


  • Options > Lighting > Flash delay
    The parameter "Flash delay" of the internal or external lamp was without function. When restoring data backups of previous firmware versions, this parameter for "other" lamps is therefore set to the value zero.


  • Program sequence
    During processing of program sequences, with certain operating sequences, it could happen that the user interface no longer responded correctly.


  • PROFINET IO trigger debouncing
    For triggers via PROFINET IO the set debounce time was not correctly applied. Depending on the setting and trigger interval, this could result in too much or too little trigger being accepted.

Please refer to the RelNotesDE/RelNotesEN.

 

Compatibility:

  • Firmware version 1.2 is fully backward compatible with the previous version 1.1.
  • The programs of the previous version can be taken over without changes.

 

Hardware to use the new firmware: 

Product name

Order number

SIMATIC MV540 S

6GF3540-0CD10

SIMATIC MV540 H

6GF3540-0GE10

SIMATIC MV550 S

6GF3550-0CD10

SIMATIC MV550 H

6GF3550-0GE10

SIMATIC MV560 U

6GF3560-0LE10

 

Third-party software – license conditions and copyright information

You can find the copyright information for the third-party software contained in this product, particularly open source software, as well as applicable license conditions of such third-party software in the ReadMe_OSS file.

Special note for resellers

The information and the license conditions in the Readme_OSS file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

 Registrierung notwendig  Siemens_Third-Party_Software_disclosure_document.html (8.4 MB)

 

Download of SIMATIC MV500 V1.2.0 firmware:

 Download unterliegt Exportcontrolle  MV500_V01.02.00.zip (95.6 MB)

 

The download includes:

  • MV500 Firmware Version  1.2.0
  • GSDML files
  • Documentation (operating instructions (compact), operating instructions),
  • Siemens Third-Party Software disclosure document.html,
  • RelNotesEN and RelNotesDE (please read prior to installation)

 

Important: The complete documentation for the products SIMATIC MV540, SIMATIC MV550 and SIMATIC MV560 is available in the download.

 
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.