×
Siemens Industry Online Support
Siemens AG
Type bericht: FAQ ID van bericht: 109772250, Datum bericht: 09/22/2021
(1)
Beoordelen

Parameter transfer from SIMARIS Design to communication-capable 3VA molded case circuit breaker

  • Bericht
  • Heeft betrekking op product(en)
Instructions for transferring the data (.sd file) of a planned power-distribution system from SIMARIS Design to communication-capable systems by means of the commissioning software powerconfig (.sx file) using the example of the 3VA molded case circuit breaker.

[click to enlarge the images]


1. Conversion of the SIMARIS .sd file to .sx file.



2. Creating a new project in the powerconfig commissioning software
 



3. Click on "Project".




4. Go to "Edit" and then select "Import device(s)..."



5. Select the desired *.sx file.



 
6. "Search for available device..." to create the COM100, or COM800 modules.




 
7. Select COM800/100 module(s) and then select "Load selected device(s) in PC".



 
8. Use the mouse to drag the appropriate switches from the Gateway hierarchy into the associated COM module.


 
9. Mark COM800/100, go online and click on the "Overview" [eye symbol].



10. Then the new switches with the default address 126 (factory setting) will be loaded.


 
Select switch.
11.  Switch to "Flashing mode" in order to identify the switch in the system so that this built-in switch also receives the corresponding




12. Parameters from SIMARIS Design later on.


 
13. Select "Start flashing" in order to activate the ACT and COM LEDs on the switches concerned. After a successful test, select "Stop flashing" to close the window.




14. Click on "Device Name", select the appropriate switch from the "Drop Down" menu so that the SIMARIS parameters are later transferred to the correct switch at the installation site.


 
15. Click on "Switch address" and provide an address e.g., 1 for LS1.1A.4B. The same procedure also applies to other switches.


 
16. Select both switches (Ctrl) and confirm the configuration of the selected switches.



 
17. Select both switches (WARNING! Do not confirm "Load selected breakers to PC"!! Otherwise the SIMARIS parameters will be overwritten by the default values of the switch!) and click on Synchronize and go offline ["Go Offline"].




18. Click on "Communication" (1.), "unlock" processing field (2.), change switch address (3.) – e.g. change 126 to 1. Finally load the communication parameters to the PC (4.) and "lock" editing (5.)    




19. Note: If this messages appears, you may have selected an incorrect switch. Please open "Details" and read the error message.




20. If no warning message appears, select "Parameters" and load the SIMARIS parameters to the switch.



21. Recommendation: To check the parameters, you can also upload the values again.

Nota's in verband met security
Ter bescherming van technische infrastructuur, systemen, machines en netwerken tegen digitale dreigingen is het noodzakelijk om een alomvattend 'IT Security' concept te implementeren (en continu te handhaven) dat overeenkomt met de huidige stand van de techniek. De producten en oplossingen van Siemens vormen slechts een klein deel van een dergelijk concept. Meer informatie over 'Cyber Security' vindt u op
https://www.siemens.com/cybersecurity#Ouraspiration.
Bericht beoordelen
geen beoordeling
Verzoeken en feedback
Wat wilt u doen?
Opmerking: de feedback heeft altijd betrekking op het actuele artikel/product. Uw bericht wordt naar de technische redacteurs van de Online Support gestuurd. We zullen binnen enkele dagen antwoorden als uw feedback dat vereist. Als we geen vragen meer hebben, zullen we geen antwoord meer sturen.