×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109772314, Entry date: 07/12/2021
(2)
Rate

Overview of the engineering functions supported in Startdrive V15.1, V16 and V17 with SINAMICS DCC V15.1 and V16

  • Entry
  • Associated product(s)
Overview of the engineering functions of SINAMICS DCC V15.1, V16 and V17

SINAMICS DCC (Drive Control Chart) is a technological enhancement of SINAMICS S120/S150/G130/G150 drives systems. It enables  the device functionality of the drive systems to be individually expanded by freely available closed-loop control, arithmetic and logic blocks.

The user-friendly configuration tool SINAMICS DCC V15.1/V16/V17 facilitates easy graphical configuration of the blocks and their integration in the drive unit. SINAMICS DCC V15.1/V16/V17  provides users with a new level of versatility when adapting these systems to the specific functions of their machines. It enables complex applications such as for winders or traversers to be implemented.  

Note
Startdrive V15.1, V16 and V17, the same version of SINAMICS DCC and SINAMICS firmware >=V5.2 are required to use SINAMICS DCC .

Download
  109772314_SINAMICS_DCC_V17_Supported_Functions_en.pdf (44,2 KB)
  109772314_SINAMICS_DCC_V16_Supported_Functions_en.pdf (234,7 KB)
  109772314_SINAMICS_DCC_V15_1_Supported_Functions_en.pdf (2,4 MB)

Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.