×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109772751, Entry date: 11/04/2019
(0)
Rate

DTM: SITRANS Probe LU240 - HART V7 - SITRANS DTM 4.1

  • Entry
  • Associated product(s)

Engineering Tool

SITRANS DTM




Tool Version

4.1

Supported Firmware:

1.01.02

EDD-Version:

1.01.00-02

Order Number:

7ML511*-***0*-4***

Hardware-Version:

1.00.00

Firmware-Version:

1.01.02

 

To use this DTM package SITRANS DTM needs to be installed first.

This is the Device Type Manager (DTM) for SITRANS Probe LU240 for FDT Frame applications (e.g. PactWare) with SITRANS DTM 4.1

For more information please check: https://www.siemens.com/sitransprobelu240.


New features in this update:
- Added datalogging


SITRANS DTM - powered by EDDL
This installation file requires the software SITRANS DTM. SITRANS DTM has to be installed only once and can be downloaded from product support under the following links:
SITRANS DTM 3.1:  53754140 
SITRANS DTM 4.1:  109484287 

After the installation of SITRANS DTM, any desired device DTM can be installed. To install the device DTM,  unzip it, then double-click on the .exe file and follow the instructions.
More information about the installation can be found under the following link: 61705616 

 Registrierung notwendig  SITRANS_PROBE_LU240_HA_DTM_FDT_1_01_00_02.zip (1,2 MB)

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.