×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109773688, Entry date: 12/09/2019
(0)
Rate

Delivery release of Telecontrol Patch for SIMATIC STEP 7 Professional / Basic V16.0

  • Entry
  • Associated product(s)
Telecontrol Patch V16 (patch DLL) for STEP 7 V16.0 is hereby released.

Note on Telecontrol configuration with DNP3 and IEC 60870

 

A patch must be installed to use the Telecontrol configuration with DNP3 and IEC 60870 in SIMATIC STEP 7 Professional / Basic V16.0. This patch is now available from Siemens Technical Support Services.

As soon as Update 1 of STEP 7 V16.0 is available, the patch no longer needs to be installed.

Please read the notes in the patch readme.

 

See also delivery release for SIMATIC STEP 7 Professional / Basic V16 from 02.12.2019: 109771628 


 
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.