×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109775566, Entry date: 01/24/2020
(0)
Rate

SIMATIC Robot Integrator for standard Kinematics - Getting Started

  • Entry
  • Associated product(s)

With the release of TIA Portal V15 and the firmware V2.5 the technology object “Kinematics” was introduced into the SIMATIC S7-1500 Technology CPU. This system integrated Motion Control functionality allows to control and coordinate kinematics with up to 4 interpolating axes (X-, Y-, Z- and orientation axis A). Among other things, these can be used in TIA Portal to control kinematics via a separate control panel and to generate a path movement.
In the application example is shown, how the implementation via a mobile and a comfort panel with the corresponding PLC program could look like.

This Getting Started contains the programming of 2-4-axes kinematics using a SIMATIC S7-1500 T-CPU by means of a technology object.

It provides you with numerous functions which are also accessible from the included HMI. Among others you will find the following functions on the HMI:

  • Jogging the kinematics
  • Teaching of singular positions
  • Teaching and moving on complete trajectories with editable transition conditions
  • Configuration of tool and base coordinate systems
  • Visualization of the kinematics’ diagnostic data
  • Switching languages between English and German

Below you can find selected screenshots of the HMI of the KTP900F.


Fig. 1: Start screen


Fig. 2: Move kinematics


Fig. 3: Move on path

Every functionality realized in the application example is available for all kinematics supported by the technology object “Kinematics”.
In the application example two HMIs with identical functions are also included. They are optimized for the TP1500 Comfort Panel and the KTP900F Mobile Panel.
The corresponding documentation explains step by step how to use the application example and describes the structure in TIA Portal. Afterwards the answers to various problems and frequently asked questions are given.

Further information
To access the Getting Started open a Support Request using the keyword "SIMATIC Robot Integrator for Standard Kinematics".

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.