×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109777633, Entry date: 12/07/2021
(6)
Rate

Startdrive V16/V17: Edit parameters in several drives Add-In

  • Entry
  • Associated product(s)
TIA Portal V16/17 facilitates the commissioning of similar drives by copying an existing configuration from one drive object to other drive objects. Parameter values can be written offline or online.

In applications such as logistics systems or in the automobile industry, oftentimes more than 100 drives are controlled by one PLC. In materials handling applications, for instance, drive settings are often standardized for various conveyor elements. In such cases, the configurations are the same, or they differ only with respect to parameters that are not performance-related.

When commissioning such a system it is repeatedly the case that settings parameters have to be adjusted in order to achieve the desired drive characteristics. These changes then have to be carried out for a great number of drives (10 to 50). Although these are simple changes, they take considerable time.

 
TIA Portal Add-In "EditParametersInSeveralDrives"
The TIA Portal add-in "EditParametersInSeveralDrives" facilitates the commissioning of similar drives by copying an existing configuration from one drive object to other drive objects.  

You can enjoy the following benefits by using the TIA Portal add-in "EditParametersInSeveralDrives":
  • Reduce commissioning time
  • Change parameters even without knowledge of TIA Portal
  • Prevent errors with the help of automatic processing



The TIA Portal Add-in "EditParametersInSeveralDrives" offers the following functions:

  • Display the drives in the project
  • Support for drives from the SINAMICS S120, S210, G120, G120 and G110 series
  • Support for SINAMICS G120X drives (as of TIA Portal V17)
  • Read and write drive parameters offline and online
  • Compare parameter values of multiple drives offline and online
  • Support for hardware parameters (DFI: Drive Function Interface)


Downloads
  Documentation for TIA Portal V17 (2,6 MB)
 Registrierung notwendig  Add-In for TIA Portal V17 (4,4 MB)
 Registrierung notwendig  Visual Studio Project / Source Code of the Add-In for TIA Portal V17 (7,3 MB)(SHA-256)


  Documentation for TIA Portal V16 (2,2 MB)
 Registrierung notwendig  Add-In for TIA Portal V16 (2,5 MB) 
 Registrierung notwendig  Visual Studio Project / Source Code of the Add-In for TIA Portal V16 (958,1 KB)(SHA-256)


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.