×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109778281, Entry date: 08/31/2020
(2)
Rate

SIWAREX WP351 example project „ready-to-use”

  • Entry
  • Associated product(s)

SIWAREX WP351 – Example project for legal-for-trade applications

The following TIA Portal project contains the WP351 SIMATIC function block for S7-300/400, S7-1200, S7-1500 and ET 200SP Open Controller. An HMI visualization (TP700 Comfort), which allows full access to the scale, is contained too. If the HMI shall be integrated into an existing HMI, the following steps need to be considered:

  1. Copy all PLC data types and all function and data blocks from the example project into the target project.

  2. Copy the complete HMI from the example project into the target project.

  3. Copy all screens, screen templates, Pop-Up screen, Slide-In screens, variables und scripts from the WP351 HMI into your target HMI.

  4. Reconnect all WP351 variables to the new „Interface“ data block in your target controller.

  5. Download on 109477602 the SecureDisplay and parametrize it according the enclosed documentation.


SIWAREX WP351 – Example project not legal-for-trade.

The following TIA Portal project contains the WP351 SIMATIC function block for S7-300/400, S7-1200, S7-1500 and ET 200SP Open Controller. An HMI visualization (TP700 Comfort), which allows full access to the scale, is contained too. If the HMI shall be integrated into an existing HMI, the following steps need to be considered:

  1. Copy all PLC data types and all function and data blocks from the example project into the target project..
  2. Copy the complete HMI from the example project into the target project.
  3. Copy all screens, screen templates, Pop-Up screen, Slide-In screens, variables und scripts from the WP351 HMI into your target HMI.
  4. Reconnect all WP351 variables to the new „Interface“ data block in your target controller.


SIWAREX WP351 – Example project to program several Siwarex WP351 in one project, not legal for trade

The TIA Portal Project is based on the example project for not legal-for-trade applications, it has been developed in order to connect several scales to a 1500-CPU or 1200-CPU which is connected to a panel. This   document (4,7 MB) describes the procedure.




SIWAREX WP351 Library for Siwarex WP351 to limit the simultaneously use of system function data record read and / or write

The library is created for 1200 and 1500 CPU’s. The function block “WP351_Token” is an extension of the “WP351_Multiplex” getting started. This   document (531,1 KB) describes the procedure.




 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.