×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109778305, Entry date: 03/05/2020
(4)
Rate

Firmware V6.2 for SCALANCE M-800 / S615

  • Entry
  • Associated product(s)
Firmware V6.2 for SCALANCE M-800 / S615 is now available for download.

The following features have been added:

Personalized welcome message

  • A message can be uploaded, which is shown on the login page.

Display SSH fingerprint

  • Information > Security Overview now display the SSH fingerprints.

Configurable server ports

  • The default ports used for HTTP, HTTPS, Telnet, SSH and SNMP are now configurable.

Password when loading and saving the configuration

  • Loading and saving of Config and Config Pack can now be secured by passwords.

DHCP Client M-800

  • DHCP Client is now supported on all SCALANCE M-800 devices.

Wizard extension – for SHDSL modem

  • DHCP Client is included in the wizard.

Connection monitoring – Extension

  • The connection monitoring with the associated restart or reset actions has been fundamentally revised.

Scheduled restart

  • A restart can be triggered by a timer on the System > Restart page.

NAT rules – NETMAP extensions

  • NETMAP rules can be edited
  • Check box introduced for automatic creation of bidirectional rules
  • Check box introduced for automatic creation of firewall rules associated with NETMAP rules

User-specific firewall rules extension

  • User-specific firewall rules can now be used in combination with the "Valid login" and "Digital input active" events

Pre-defined IPv4 rules extended

  • The pre-defined IPv4 rules can now also be used for PPPoE interfaces, VRRP interfaces and VPN connections.

Passwords for Config files

  • Config and Config Pack can be protected with a password before downloading.

IPsec – Extension

  • When using IKEv2, more than one subnet can be entered for the remote endpoints and connections.

SINEMA RC, IPsec, OpenVPN – Extension

  • You can now set a time after which the unused VPN tunnels are terminated.

Detection of IP address collisions

  • The function for detecting and reporting IP address collisions is supported.

DHCP server – Static assignments

  • A comment column has been introduced.

Syslog Client – Extension

  • Syslog messages can now also be sent TLS-encrypted over TCP.

 

In addition for SCALANCE M-800:

SMS Relay – Extension for sending SMS

  • SMS can be sent from the device, e.g. to activate SMS-based services such as "Email2SMS".

Mobile data use

  • A display for the consumed data volume was introduced.

 

The following configuration limits have been increased:

DHCP – Static allocations per DHCP pool

  • The configuration limit for static IP addresses was extended to 128 per pool.

 

Changes were made in the following areas:

IPsec - Improved performance when setting up IPsec tunnels

  • Relevant when using multiple IPsec tunnels on one device.

Events – Digital input

  • All digital input events will be active by default in the future. When firmware is updated, the settings valid at that time are retained.

 

Corrections have been made in the following areas:

VRRPv3 – Relevant when using the function

  • When using VRRPv3, devices may sporadically reboot.

PPPoE – Relevant for the configuration of the function

  • In WBM, no static IP address could be created on the PPP interface.

 

Security information:

This update contains security-relevant changes which enhance robustness against possible attacks. We therefore recommend that you update the firmware.

 

Security fixes and improvements:

Correction of SSA-462066: Vulnerability known as TCP SACK PANIC in Industrial Products

Firmware update V6.2 has been released for upgrading the following product versions:

 

SCALANCE M804PB

6GK5804-0AP00-2AA2

SCALANCE M812-1 (ANNEX A)

6GK5812-1AA00-2AA2

SCALANCE M812-1 (ANNEX B)

6GK5812-1BA00-2AA2

SCALANCE M816-1 (ANNEX A)

6GK5816-1AA00-2AA2

SCALANCE M816-1 (ANNEX B)

6GK5816-1BA00-2AA2

SCALANCE M826-2

6GK5826-2AB00-2AB2

SCALANCE M874-2

6GK5874-2AA00-2AA2

SCALANCE M874-3

6GK5874-3AA00-2AA2

SCALANCE M874-3 (CN)

6GK5874-3AA00-2FA2

SCALANCE M876-3

6GK5876-3AA02-2BA2

SCALANCE M876-3 (ROK)

6GK5876-3AA02-2EA2

SCALANCE M876-4 (EU)

6GK5876-4AA00-2BA2

SCALANCE M876-4 (NAM)

6GK5876-4AA00-2DA2

SCALANCE S615

6GK5615-0AA00-2AA2

RUGGEDCOM RM1224 LTE(4G) EU

6GK6 108-4AM00-2BA2

RUGGEDCOM RM1224 LTE(4G) NAM

6GK6 108-4AM00-2DA2

 

 

Third-party software – license conditions and copyright information

You can find the copyright information for the third-party software contained in this product, particularly open source software, as well as applicable license conditions of such third-party software in the ReadMe_OSS file.

Special note for resellers

The information and the license conditions in the Readme_OSS file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.
   OSS_SCALANCE-M-800-S615_86.pdf (11.4 MB)

Please read the product documentation for installation.

 

You can download the file here.

 Registrierung notwendig  firmware_SCALANCE_M800_S615_V06.02.00.zip (27.1 MB)

Hash:  Registrierung notwendig  firmware_SCALANCE_M800_S615_V06.02.00.zip_SHA256.txt (1 KB)

You can download the private MIB here.

 Registrierung notwendig  scalance_m_msps_mib.zip (163.0 KB)

Hash:  Registrierung notwendig  scalance_m_msps_mib.zip_SHA256.txt (1 KB)

 

You can find the source code of the Open Source Software here:

 Registrierung notwendig  M800_S615_V06.02.00_oss.zip (230.7 MB)

Hash:  Registrierung notwendig  M800_S615_V06.02.00_oss.zip_SHA256.txt (1 KB)

 

Cell firmware SCALANCE M874-3:

You can download the file here.

 Registrierung notwendig  firmware_Cell_M874-3_V03p320p6.zip (10.0 MB)

Hash:  Registrierung notwendig  firmware_Cell_M874-3_V03p320p6.zip_sha256.txt (1 KB)

 

ADSL firmware SCALANCE M812/M816: 

Annex A

You can download the file here.

Please note that the device firmware must be installed first.

 Registrierung notwendig  Annex_A_V01.01.00.00_03.01.01.zip (8.0 MB) 

Hash:  Registrierung notwendig  Annex_A_V01.01.00.00_03.01.01.zip_SHA256.txt (1 KB)

 

Annex B

You can download the file here.

Please note that the device firmware must be installed first.

 Registrierung notwendig  Annex_B_V01.01.00.00_03.01.01.zip (8.0 MB)

Hash:  Registrierung notwendig  Annex_B_V01.01.00.00_03.01.01.zip_SHA256.txt (1 KB)

 

Contact for technical issues: Customer Support, DI CS SD CCC TS, Contact form

 
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.