×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109779004, Entry date: 03/31/2020
(0)
Rate

Delivery release firmware V2.8 for TIM 4R-IE including download

  • Entry
  • Associated product(s)
The firmware V2.8 for the SINAUT communication module TIM 4R-IE is released and available for download effective immediately. The module is scheduled for delivery as of June 2020 with firmware V2.8.

1. Product description  

The firmware V2.8 includes the following new functions and product improvements:

  • Support of S7-Routing via TIM 4R-IE when configuring in the TIA Portal.

  

Security information

This version contains security-related improvements which improve ruggedness. An update is recommended.  


Correction of SSA-359303: Debug Port in TIM 3V-IE and 4R-IE Family Devices

https://cert-portal.siemens.com/productcert/pdf/ssa-359303.pdf

 


2. Firmware update  

Save the file in a temporary folder. The installation is started automatically when the .exe file is unzipped.

 

The firmware, consisting of

  • the basic package TIM4RIE_V2.8.FWL for the TIM 4R-IE and
  • the driver package, which must be loaded onto the TIM 4R-IE,

 

is then stored automatically in the folder ...\P7ST\TIMFW_VXW4R under the STEP 7 installation environment.

 

The basic package and the driver package of the TIM 4R-IE firmware must be loaded onto the TIM module with two different programs in the order described here:

 

1. Driver package

To load the driver package, the SINAUT Diagnostics and Service tool must be used.

No file or path information is necessary to load the driver package. The driver package is found automatically.

 

2. Basic package

To load the basic package, use the NCM Firmware Loader.

(Component of STEP 7: SIMATIC => STEP 7 => NCM S7 => Firmware Loader).

To load the basic package with the NCM Firmware Loader, you need to know the correct file name and file path (e.g.....\P7ST\TIMFW_VXW4R/TIM4RIE_V2.8.FWL) because this must be specified explicitly in the NCM Firmware Loader.

 

Please note that the basic package may only be loaded over the Ethernet interface of the TIM and the MAC address must be known (see sticker behind the front flap of the TIM). The S7 online interface of your programming device/PC must be set to "ISO Ind. Ethernet" in the "Set PG/PC interface" dialog.  

To load the basic package, the TIM module must be put in download mode. For this you need to briefly press the Reset button of the TIM. The TIM will then begin to restart, which is indicated by the fact that the TIM switches on all LEDs for about 5 seconds. You must press the Reset button of the TIM again within this time and hold it until the RUN LED of the TIM starts to flash. The TIM is then in download mode. The download can now be started via the NCM Firmware Loader. As soon as the download is activated by the Firmware Loader, the STOP LED of the TIM starts to flash and flashes until the download procedure is complete. A voltage reset must be carried out after this.

 

For more detailed information, refer to the Readme file which is part of the extracted firmware.

 

2. Ordering data  

Product name

Order number

SINAUT Module TIM 4R-IE

6NH7800-4BA00

 

3. Additional information  

The TIM firmware V2.8 is backward compatible to previous versions.

 

4. Download of firmware V2.8 for TIM 4R-IE  

Third-party software – license conditions and copyright notes

You can find the copyright notes on the third-party software, especially Open Source Software, contained in this product as well as applicable license conditions for this type of third-party software in the following ReadMe file.

Special note for resellers

The information and the license conditions in the readme file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

  OSS_TIM-4RIE_99.pdf (1.2 MB)

 

Download FW V2.8.0:

 Registrierung notwendig  TIMFW4RIE_V2.8.0_OSS.zip (10.9 MB)

 

 
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.