×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109779181, Entry date: 08/09/2021
(1)
Rate

What’s new | SIMATIC Performance Insight MindSphere app August 2021

  • Entry
  • Associated product(s)
Learn more about new features and changes in our recent update
What’s new | SIMATIC Performance Insight MindSphere app August 2021

The following changes are provided
  • Aggregated values are displayed in the middel of the time periode instead of the period end in the chart widget. In the Tooltip the user can see the From-To period.
  • Small Bug Fixes & Usability Improvements 

What’s new | SIMATIC Performance Insight MindSphere app June 2021

The following changes are provided
  • Extension of the zoom function in the Chart widget or in the Detail view of all widgets. The user can zoom in and out in stages.
  • Widgets can now also be copied.
  • A CSV data export can be performed directly from the widget.
  • Administrator privileges are now also supported for subtenant users for the  configuration of KPI instances and dashboards.
  • Small Bug Fixes & Usability Improvements 

What’s new | SIMATIC Performance Insight MindSphere app March 2021

The following changes are provided
  • A pre-defined dashboard for OEE analysis of machines and plants is available. The configuration can be easily performed with just a few clicks on the corresponding asset.





  • The essential KPIs (TEEP, OEE, performance, availability, quality, MTTR as well as the MTBF) are displayed to the user. The key performance indicators of the previous period are shown as a reference for better classification of the displayed results. In the detail view, the most important KPIs are displayed to the user in a line diagram. In the histogram view, the statistics information is displayed, and in the time comparison view, the OEE, performance, availability and quality KPIs are displayed for yesterday, last week and last month.
  • For KPI instances that are automatically generated, the user can define the limits, whereby limits are defined by default that are also used in the pre-defined dashboard.
  • In the Gantt chart, the user obtains an overview of the corresponding machine states, the frequency and the duration for which the state has been present. In the detail view, the user is additionally offered the analysis of the time model.
  • The pricing model has been extended by the number of assets for the OEE analysis. In addition to the KPIs and the users, the OEE analysis is now also taken into account in the pricing. The KPI instances generated for the OEE analysis are included in the assets for OEE analysis price point and are therefore not included in the number of KPIs.
  • Data (time series) with a Quality Code Flag not equal to OK are not considered in the display or in the KPI calculation.
  • An extended Gantt chart with zoom function is available.
  • Small Bug Fixes & Usability Improvements 
 

What’s new | SIMATIC Performance Insight MindSphere app November 2020

The following changes are provided
  • A pre-defined time category model is available.
         

  • For each machine state the user can define the appropriate time category
  • This configuration is used to calculate how long the machine is in a dedicated time category or how often one of the assigned machine states is in a dedicated time category.
  • Pre-defined KPI Types are available  (TEEP, OEE, Availability, Performance, Quality, MTTR, MTBF)
  • Small Bug Fixes & Usability Improvements 

What’s new | SIMATIC Performance Insight MindSphere app August 2020

The following changes are provided
  • With this update, limits for variables of type String and Boolean can be defined, monitored and notified.
  • Small Bug Fixes & usability Improvements

What’s new | SIMATIC Performance Insight MindSphere app July 2020

The following changes are provided:
  • With the new function "Activate notification", you can define upper and lower limit values ​​for variables and KPI instances, which trigger a notification if these limit values ​​are exceeded or undershot. The notification is displayed in the SIMATIC Notifier MindSphere app and sent directly to the desired mobile device. 
  • The limits ​​defined on the variable or KPI instance are inherited by default to the widget configuration.
  •  


What’s new | SIMATIC Performance Insight MindSphere app April 2020

The following changes are provided:
  • A data reduction algorithm is used to efficiently display high-frequency data in the "Diagram" widget This algorithm reduces the data to a specific amount so that it can be displayed. With the update, the affected detail data is now reloaded when zooming. 
  • When you change a widget, you can now jump back and forth between the individual tabs directly in the wizard.
  • Small Bug Fixes & usability Improvements
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.