×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109780220, Entry date: 05/29/2020
(0)
Rate

SINAMICS V20: When use USS/Modbus to control V20, it can't start up directly

  • Entry
  • Associated product(s)
When the drive is in "ON Inhibit" state (r2=6), it must get the switch off command to get in "Ready" state.

​When you use "USS/MODBUS on RS485" as control resource (p700=5), the SINAMICS V20 can be in "ON Inhibit" state and does not switch on in below situations:

  • Situation 1: The communication is not established between Host device and SINAMICS V20
  • Situation 2: F72 occurs, and the fault is not reset

This "ON Inhibit" statue prevents the SINAMICS V20 from a direct start-up. In this case, r2 shows the value 6.
The bits "ON/OFF1" and "Acknowlege" need a signal change from false to true to execute there function.

To start the drive you have to:

  • Set "ON/OFF1" bit to false and "Acknowlege" bit to true
    This will change from state "On Inhibit" to "Ready" (r2=1)
  • Set "ON/OFF1" bit to true to start the drive ( It's recommended to reset "Acknowlege" bit to false)

Typical sequence for USS in the control word is:

  • 16#04FE - switch off ("ON/OFF1" (bit 0) = false, "Acknowledge" (bit 7) = true, all other enables are set)
    This will change from state "On Inhibit" to "Ready" (r2=1)
  • 16#047F - switch on ("ON/OFF1" (bit 0) = true, "Acknowledge" (bit 7) = false, all other enables are set)

Typical sequence for Modbus RTU is:

  • Set register 40006 to 0 (Switch off) and register 40007 to 1 (Acknowledge faults)
    This will change from state "On Inhibit" to "Ready" 
    (r2=1)
  • Set register 40006 to 1 (Switch on) and register 40007 to 0 (Prepare new acknowledge )

The register 40004 must be 1 for operation (RUN enable).


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.