×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109780760, Entry date: 08/04/2020
(9)
Rate

ABT Site V4.0 - Download Installer

  • Entry
  • Associated product(s)
This information is targeted for customers who bought Comfort devices not directly from Siemens but from a reseller of Siemens products. All other product users, Siemens internal or Siemens solution partners, must use the known and established contacts in order to get the appropriate information and deliveries.


ABT Site Engineering and Commissioning Tool - Getting Started109780756 

Download Desigo ABT Firmware library 109780759 


Installation package and requirements

Product Name: ABTSite

Product Version: ABT V4.0.0 Build 39.0.666.0

Creation/revision Date: 29.06.2020

This version contains products or applications that may not be available in particular countries.

Runtime environment

This software is designed to run on 64-bit OS only.

This ABT Build can be installed on the following operating systems:

  • Windows 10 Professional or Enterprise

Not supported is:

  • Windows 7, Windows XP, Windows Vista; any Win 32bit

Please note that the minimum system requirements are a dual core computer with at least 8 GB RAM, recommended is to have more. Also, in case of using virtual machines, please make sure that the virtual machine has this memory available.

If RAM memory on PC is not sufficient, performance goes down drastically, but no crash and no damage of project data.

 

Installation prerequisites and installation sequence

Installing or uninstalling ABT Site requires Windows Administrator access rights.

ABT Site is provided as one complete installer program, all required software components will be installed automatically.

Before installing ABT Site please make sure that there is sufficient free memory on disk C:
Lack of free memory can cause problems during use of ABT Site.

Prerequisites for installation of this build

The following prerequisites must be met before ABT Site installation:

New .Net Framework 4.7.2. required:

Install or update .Net Framework and install patches.

Restart PC before continuing with ABT installation

If .Net Framework 4.7.2 is not installed prior to the installation of ABT Site you will get an error message:

Please download .net framework 4.7.2 from here

Make sure that .Net Framework is turned on in Windows Features

It is recommended to install the most recent JRE directly from Java directly from Java:

https://www.java.com/en/download/win10.jsp

Actual JRE version: Java for Windows Version 8 Update 251 (April 2020)


New installation

  1. Download the ABT Site installation package and save it to your PC.
     Registrierung notwendig  ABT_Installer.zip (87,0 MB)
  2. Unzip the ABT Site installation package and double click on ABT_Installer.exe and follow the instructions.
  3. Restart your PC after installation.

Update installation

Update installations from 3.x to 4.x are not supported. Therefore, the Tool and the Libraries must be uninstalled separately. Uninstall all previous ABT Site and ABT Pro Library Sets manually.

  1. Archive any existing ABT Site project.
  2. Download the new installer and save to your PC.
  3. Extract the ABT Installer zip file, this will start the ABT Installer program (Wait till it initialize 3 mins)
  4. Select language and then chose "Uninstall" to uninstall any existing ABT Site version (e.g. V3.3.2).
  5. Close the installer.
  6. On your PC go the Apps and Features and uninstall any remaining ABT application libraries packages.
  7. Restart your PC.
  8. Start the installer again and install ABT Site V4.0 including your choice of application libraries for room automation and Desigo Control Point.
  9. Restart your PC again.


NOTE: The internet connection is needed during installation. Depending on your internet connectivity speed, the duration of the installation will vary.

 

Uninstall, repair and modify installation:

To repair, modify or uninstall ABT Site, just run the ABT Installer again.

We do not recommend uninstalling the tool, using Windows Apps & Features

The Tool and application language can be changed at any time. There is no need to run the installer again with with a different language preselection.


Distribution and product support

Further information is available via online support. Please comply with the following steps:

Product support

Forum

Support Request


If you have any specific questions regarding this subject, please contact your local SI BP Customer Support.
Responsible for the content of this article is the Customer Support team in Zug (TOS).

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.