×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109780910, Entry date: 07/31/2020
(0)
Rate

Sales release of SINAMICS G120XA firmware version V1.03

  • Entry
  • Associated product(s)
Effective immediately, SINAMICS G120XA firmware version V1.03 is sales released.

Affected commissioning tools

The following commissioning tools are offered for configuring SINAMICS G120XA with firmware version V1.03:

Engineering system

Production information

BOP-2

Support included in V4.7 SP10

IOP-2 V2.6

Available in Aug, 2020

G120 Smart Access V1.5

Available in Sep, 2020

 

Functional extensions

The following expanded functions are available with SINAMICS G120XA firmware version V1.03:

Function

Description

Free Function Block (FFB)

·         Integrated 16 different function types and 40 function blocks,

·         Including logical, mathematical, numerical and other free programmable function blocks.

·         Cover the requirement for controlling the drive system in a wide variety of applications

·         User-friendly commissioning with G120 Smart Access Module

 

Third-party software – license conditions and copyright notes

You can find the copyright notes on the third-party software, especially Open Source Software, as well as applicable license conditions for this type of third-party software in the file  Registrierung notwendig  Read_OSS.htm (1,5 MB).

Availability of the source code

Some license conditions of third-party software components used in this product may oblige us to provide you with the source text and further information for these components. You can find this information either directly on the product itself or with the product (e.g. on a mass storage medium, DVD). Should this not be possible due to technical reasons, Siemens will send you this OSS Source Code against payment of the handling expenses. Please contact the address specified at the end of this section regarding this matter.

Siemens AG
Customer Service DF&PD
DF CS SD CCC TS
Gleiwitzer Str. 555
90475 Nuremberg, Germany
Tel: +49 (911) 895 7222
Support

Download and upgrade

Firmware download

The SINAMICS G120XA firmware version V1.03 can be downloaded here:  Registrierung notwendig  G120X_04712723_OA_1030005_BIOS_04703703.zip (15,6 MB)

Firmware upgrade

With an SD card, you can upgrade the SINAMICS G120XA inverter with older firmware version to this firmware version by following the steps as below:

  1. Download the required firmware to your PC from the source as above. Extract the files and transfer the unzipped files into the root directory of the SD card.

  2. Switch off the converter power supply.

  3. Insert the card into the converter slot until it latches into place.

  4. Switch on the converter power supply again. The converter transfers the firmware to its memory, which takes 5 to 10 minutes. While data is being transferred, the LED RDY on the converter stays red. The LED BF flashed orange with a variable frequency.

  5. At the end of the transfer, the LED RDY and BF slowly flash red (0.5Hz). The converter firmware will be incomplete if the power supply fails during the transfer. In this case, start again with step 2.

List of fault and alarms

The “alarmlist_*.xml” files are not necessary for the correct operation of the firmware. They only include an export of the “Alarm messages” text for the SINAMICS G120XA in the “xml” format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. Therefore, as far as the SINAMICS G120XA product is connected, no additional support can be provided here.

The list of fault and alarms in 6 languages including Chinese, English, German, Italian, French and Spanish can be downloaded here:  Registrierung notwendig  Alarm_list_in_6_languages.zip (313,5 KB) 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.