×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109781019, Entry date: 12/11/2020
(0)
Rate

SINAMICS firmware version 4.7 SP13 HF2 for SINAMICS G120 (CU240B/E-2, CU250S-2), G120P (CU230P-2), G120C, G120D (CU240D-2, CU250D-2), G110M, and SIMATIC ET200pro FC-2, G115D products

  • Entry
  • Associated product(s)
In this entry you will find the download as well as the ordering information for SINAMICS G120 multicard with version V4.7 SP13 HF2

Content of the SINAMICS G120 multicard V4.7 SP13 HF2

In this entry you will find the download as well as the ordering information for SINAMICS G120 multicard with version V4.7 SP13 HF2. The associated sales information is available under 109781149.

The SINAMICS G120 multicard contains the firmware releases for the following SINAMICS G120 products: 

SINAMICS family

Product

Firmware (FW) version

Internal firmware identifier

G120P                                    

CU230P-2                                                                             

V4.7 SP13 HF2                          

V04.71.52.13                           

G120

CU240B-2
CU240E-2
CU240E-2 F
CU250S-2

V4.7 SP13 HF2  

V04.71.52.13

G120C

G120C

V4.7 SP13 HF2  

V04.71.52.13

G120D

CU240D-2
CU250D-2 

V4.7 SP13 HF2  

V04.71.52.13

G110M

CU240M 

V4.7 SP13 HF2  

V04.71.52.13

ET 200pro FC-2ET 200pro FC-2V4.7 SP13 HF2   V04.71.52.13
G115DG115DV4.7 SP13 HF2V04.71.52.13

The installed firmware version can be read out at the SINAMICS G module using parameter r0018 (internal version) or r0964 (complete device identification). From V4.7 SP10, a parameter r7844[1] is available to display the firmware version. The value contained in it, e.g. "04071300", corresponds to firmware version V4.7 SP1.

Note
With this download, you can only upgrade SINAMICS products as from the following firmware versions to V4.7 SP13 HF2:

  • from firmware V4.5 and higher: SINAMICS CU240E-2, CU240B-2, CU240D-2, CU250D-2 and G120C
  • from firmware V4.6: SINAMICS CU230P-2, CU250S-2 and G110M
  • from firmware V4.7 SP3 HF1: SINAMICS ET 200pro FC-2 

An overview of the available firmware releases for SINAMICS G is provided under: 67364620.


Third-party software – license conditions and copyright notes

You can find the copyright notes on the third-party software, especially Open Source Software, as well as applicable license conditions for this type of third-party software in the file READ_OSS.HTM file.

Special note for resellers

The notes and the license conditions contained in the READ_OSS.HTM file must be passed on to the purchaser in order to avoid the reseller and purchaser from violating the licensing conditions.

Availability of the source code

Some license conditions of third-party software components used in this product may oblige us to provide you with the source text and further information for these components. You can find this information either directly on the product itself or with the product (e.g. on a mass storage medium, DVD). Should this not be possible due to technical reasons, Siemens will send you this OSS Source Code against payment of the handling expenses. Please contact the address specified at the end of this section regarding this matter.

Siemens AG  
Digital Factory 
Customer Services DF&PD
DF CS SD CCC TS
Gleiwitzer Str. 555 
90475 Nuremberg, Germany 
Internet: 
http://www.siemens.com/automation/support-request
Tel.: +49 (911) 895 7222

    READ_OSS.HTM (1.1 MB)

  

Current list of general conditions of the SINAMICS G120 for firmware V4.7 SP13 HF2

 Registrierung notwendig  SINAMICS_V4.7_SP13_Restrictions_EN.pdf (493,1 KB) 


Functional restrictions which have been corrected for the SINAMICS G120 firmware V4.7 SP13 HF2

 Registrierung notwendig  SINAMICS_G_V_4_7_13_02_corrected_Functional_restrictions_EN.pdf (200,0 KB)

Provision of the SINAMICS G120 multicard V4.7 SP13 HF2

The content of the SINAMICS G120 multicard described above can be downloaded here:

Note:
From version V4.7 HF3, the runtime SINAMICS G120 firmware is not subject to any export restrictions as the output frequency has been limited to 550 Hz. It is not subject to the Iran embargo, and is not listed in the EC Dual Use regulation. (AL = N).
It is not a US product (ECCN = N).

Alternatively, the SINAMICS G120 multicard V4.7 SP13 (SD card) can be ordered using the following article number:
6SL3054-7TG00-2BA0.

Instructions for upgrading the SINAMICS G120 firmware:
When upgrading, please refer to the instructions given in the "Firmware upgrade" chapter in the operating instructions of the particular Control Unit.
As an example, you can find the firmware upgrade/downgrade instructions for the SINAMICS CU240E-2 here:

  FW_Upgrade_Downgrade_G120_CU240BE2_en.pdf (296,5 KB)

Note:
The zip file must be saved unpacked to the SD card in the root directory. An SD memory card with a capacity of least 256 MB must be used. Memory cards with capacities larger than 2 GB are not supported. An "empty SINAMICS SD-CARD 512 MB " can be ordered using article number 6SL3054-4AG00-2AA0.

 

List of faults and alarms

List of faults and alarms for SINAMICS CU230P-2

The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text for the SINAMICS G120P in the "xml" format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. Therefore, as far as the SINAMICS G120P product is concerned, no additional support can be provided here.

 Registrierung notwendig  alarmlist_g120_cu230p_v04714700_eng.xml (422,6 KB)

 Registrierung notwendig  alarmlist_g120_cu230p_v04714700_deu.xml (428,4 KB) 

 Registrierung notwendig  alarmlist_g120_cu230p_v04714700_chs.xml (391,1 KB)

 Registrierung notwendig  alarmlist_g120_cu230p_v04714700_esp.xml (444,6 KB)

 Registrierung notwendig  alarmlist_g120_cu230p_v04714700_fra.xml (456,2 KB)

 Registrierung notwendig  alarmlist_g120_cu230p_v04714700_ita.xml (451,0 KB)

 Registrierung notwendig  alarmlist_g120_cu230p_v04714700_rus.xml (562,4 KB)


List of faults and alarms for SINAMICS CU240B-2 and CU240E-2

The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text of the SINAMICS G120 in the "xml" format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. Therefore, as far as the SINAMICS G120 product is concerned, no additional support can be provided here.

 Registrierung notwendig  alarmlist_g120_cu240b_e_v04714700_eng.xml (605,6 KB)

 Registrierung notwendig  alarmlist_g120_cu240b_e_v04714700_deu.xml (613,5 KB)

 Registrierung notwendig  alarmlist_g120_cu240b_e_v04714700_chs.xml (558,3 KB)

 Registrierung notwendig  alarmlist_g120_cu240b_e_v04714700_esp.xml (635,6 KB)

 Registrierung notwendig  alarmlist_g120_cu240b_e_v04714700_fra.xml (655,1 KB) 

 Registrierung notwendig  alarmlist_g120_cu240b_e_v04714700_ita.xml (642,5 KB)

 Registrierung notwendig  alarmlist_g120_cu240b_e_v04714700_rus.xml (809,9 KB)


List of faults and alarms for the SINAMICS CU240D-2 and CU250D-2

The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text for the SINAMICS G120D in the "xml" format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. Therefore, as far as the SINAMICS G120D product is concerned, no additional support can be provided here.

 Registrierung notwendig  alarmlist_g120d_v04714700_eng.xml (780,5 KB)

 Registrierung notwendig  alarmlist_g120d_v04714700_deu.xml (787,3 KB)

 Registrierung notwendig  alarmlist_g120d_v04714700_chs.xml (720,1 KB)

 Registrierung notwendig  alarmlist_g120d_v04714700_esp.xml (818,0 KB)

 Registrierung notwendig  alarmlist_g120d_v04714700_fra.xml (841,9 KB)

 Registrierung notwendig  alarmlist_g120d_v04714700_ita.xml (827,3 KB)

 Registrierung notwendig  alarmlist_g120d_v04714700_rus.xml (1,0 MB)


List of faults and alarms for SINAMICS CU250S-2

The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text for the SINAMICS G120 in the "xml" format.  Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. Therefore, as far as the SINAMICS G120 product is concerned, no additional support can be provided here.

 Registrierung notwendig  alarmlist_g120_cu250s_v04714700_eng.xml (1,3 MB)

 Registrierung notwendig  alarmlist_g120_cu250s_v04714700_deu.xml (1,3 MB)

 Registrierung notwendig  alarmlist_g120_cu250s_v04714700_chs.xml (1,2 MB) 

 Registrierung notwendig  alarmlist_g120_cu250s_v04714700_esp.xml (1,4 MB)

 Registrierung notwendig  alarmlist_g120_cu250s_v04714700_fra.xml (1,4 MB)

 Registrierung notwendig  alarmlist_g120_cu250s_v04714700_ita.xml (1,4 MB)

 Registrierung notwendig  alarmlist_g120_cu250s_v04714700_rus.xml (1,7 MB)


List of faults and alarms of the SINAMICS G120C

The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text for the SINAMICS G120C in the "xml" format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. Therefore, as far as the SINAMICS G120C product is concerned, no additional support can be provided here.

  Registrierung notwendig  alarmlist_g120c_v04714700_eng.xml (475,0 KB) 

 Registrierung notwendig  alarmlist_g120c_v04714700_deu.xml (480,8 KB)

 Registrierung notwendig  alarmlist_g120c_v04714700_chs.xml (436,3 KB)

 Registrierung notwendig  alarmlist_g120c_v04714700_esp.xml (500,0 KB)

 Registrierung notwendig  alarmlist_g120c_v04714700_fra.xml (514,9 KB)

 Registrierung notwendig  alarmlist_g120c_v04714700_ita.xml (505,8 KB)

 Registrierung notwendig  alarmlist_g120c_v04714700_rus.xml (639,4 KB)


List of faults and alarms of the SINAMICS G110M

The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text of the SINAMICS G110M in the "xml" format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. Therefore, as far as the SINAMICS G110M product is concerned, no additional support can be provided here.

 Registrierung notwendig  alarmlist_G110M_v04714700_eng.xml (510,9 KB)

 Registrierung notwendig  alarmlist_G110M_v04714700_deu.xml (517,5 KB)

 Registrierung notwendig  alarmlist_G110M_v04714700_chs.xml (470,2 KB)

 Registrierung notwendig  alarmlist_G110M_v04714700_esp.xml (537,5 KB)

 Registrierung notwendig  alarmlist_G110M_v04714700_fra.xml (553,8 KB)

 Registrierung notwendig  alarmlist_G110M_v04714700_ita.xml (544,2 KB)

 Registrierung notwendig  alarmlist_G110M_v04714700_rus.xml (685,8 KB)


List of faults and alarms of the SIMATIC ET200pro FC-2

The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text of the SIMATIC ET200pro FC-2 in the "xml" format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. Therefore, as far as the SIMATIC ET200pro FC-2 product is concerned, no additional support can be provided here.

 Registrierung notwendig  alarmlist_et200pro_v04714700_eng.xml (526,0 KB) 

 Registrierung notwendig  alarmlist_et200pro_v04714700_deu.xml (533,4 KB) 

 Registrierung notwendig  alarmlist_et200pro_v04714700_chs.xml (482,5 KB) 

 Registrierung notwendig  alarmlist_et200pro_v04714700_esp.xml (553,4 KB) 

 Registrierung notwendig  alarmlist_et200pro_v04714700_fra.xml (570,4 KB) 

 Registrierung notwendig  alarmlist_et200pro_v04714700_ita.xml (560,3 KB) 

 Registrierung notwendig  alarmlist_et200pro_v04714700_rus.xml (712,1 KB) 


List of faults and alarms of the SINAMICS G115D

The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text of the SINAMICS G115D in the "xml" format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. Therefore, as far as the SINAMICS G115D product is concerned, no additional support can be provided here.

 Registrierung notwendig  alarmlist_G115D_v04714700_eng.xml (490,2 KB) 

 Registrierung notwendig  alarmlist_G115D_v04714700_deu.xml (496,3 KB) 

 Registrierung notwendig  alarmlist_G115D_v04714700_chs.xml (450,0 KB) 

 Registrierung notwendig  alarmlist_G115D_v04714700_esp.xml (515,8 KB) 

 Registrierung notwendig  alarmlist_G115D_v04714700_fra.xml (532,0 KB) 

 Registrierung notwendig  alarmlist_G115D_v04714700_ita.xml (522,5 KB) 

 Registrierung notwendig  alarmlist_G115D_v04714700_rus.xml (659,9 KB))


GSD files for project integration into the PROFIBUS configuring tool

PROFIBUS GSD files can be downloaded in the following entries:


GSDML files for integrating projects into the PROFINET configuring tool

PROFINET GSDML files can be downloaded in the following entries:


EDS files for integrating projects into the CANopen configuring tool

The EDS files for integrating projects into the CANopen configuring tools can be downloaded under 48351511.

EDS files for Ethernet/IP communication

The EDS files for Ethernet/IP communication can be downloaded under 78026217 


STARTER

Within the scope of SINAMICS firmware version V4.7 SP13 HF2, STARTER V5.4 HF1 (see 26233208) must be used with the SINAMICS Support Package (SSP). SSP is available under 109477753.

With SSP, new functional features in firmware V4.7 SP13 H2 can be configured using STARTER.

As part of the revision and simplification of the commissioning wizards, the SINAMICS application classes "Standard Drive Control", "Dynamic Drive Control" and "Expert" were introduced with STARTER V4.4 SP1 and SINAMICS G firmware V4.7 SP3. For additional information, refer to 109480663 .


Startdrive

Within the scope of SINAMICS firmware version V4.7 SP13 HF2, Startdrive V16 including the Hardware Support Package (HSP) V4.7 SP13 HF2 should be used (see 109771710). It is also possible to use Startdrive V15.1 (see 109760845) with the corresponding Hardware Support Package (HSP) V4.7 SP13 HF1 (see 109769122).

When importing the Hardware Support Package into an existing Startdrive V16/15 installation, new functions in V4.7 SP13 HF2 can be used with Startdrive.

As part of the revision and simplification of the commissioning wizards, the SINAMICS application classes "Standard Drive Control", "Dynamic Drive Control" and "Expert" were introduced with Startdrive V13 SP1 and SINAMICS G firmware V4.7 SP13 HF1. Additional information should be taken from the Entry 109480663 .


IOP-2/BOP-2

The HMI device IOP-2 (Article No.: 6SL3255-0AA00-4JA2) with firmware V2.6 supports the expanded functions of the SINAMICS G firmware V4.7 SP13 HF2. A complete list of the expanded functionality for IOP-2 V2.6 can be taken from the release for sale and delivery 109762019. In order to upgrade an existing IOP-2, the entry also includes an IOP-2 firmware download.

The BOP-2 operator panel (Article No.: 6SL3255-0AA00-4CA1) is automatically updated when using firmware V4.7 SP13 HF1.

As part of the revision and simplification of the commissioning wizards, the SINAMICS application classes "Standard Drive Control", "Dynamic Drive Control" and "Expert" were introduced with SINAMICS G firmware V4.7 SP3. For additional information on this subject please refer to entry 109480663 .

 
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.