×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109781070, Entry date: 07/28/2020
(3)
Rate

Firmware V6.3 for SCALANCE M-800 / S615

  • Entry
  • Associated product(s)
Firmware V6.3 for SCALANCE M-800 / S615 is now available for download.

The following features were added: 

TIA Portal Cloud Connector

  • The TIA Portal Cloud Connector enables access from an Engineering PC with TIA Portal to an Ethernet interface of a SCALANCE M800 / S615 and connected SCALANCE / SIMATIC hardware. This access is also possible in combination with VPN, e.g. with SINEMA Remote Connect.
  • Via remote TIA Portal Engineering it is possible to perform, for example, initial commissioning with an initial assignment of an IP address of the devices or also go "online" directly to the SIMATIC components.
  • The TIA Portal Cloud Connector is released in connection with TIA Portal V16 and max. 50 connected devices to SCALANCE M800 / S615 components. The runtime of an active Cloud Connector connection should not exceed the duration of a typical service assignment. 

Connection fallback

  • For Internet access, in addition to the mobile wireless connection, a LAN interface can be configured as primary Internet connection in the mobile wireless router SCALANCE M876-4. If this fails, because a previously freely configured IP address in the internal network or Internet can no longer be reached, the SCALANCE M876-4 automatically switches to the mobile wireless connection and restores the Internet connection.
  • The automatic switchover of connection between several LAN interfaces can also be configured in the SCALANCE S615.

OpenVPN extensions

  • For additional authentication of an OpenVPN connection, a TLS Static Key (PSK) can be used. In this case, incoming TLS packages are only accepted if they were signed with the TLS key.
  • Authentication on an OpenVPN server can be performed using a user name / password and certificate.

 IPsec extensions

  • Adjustable timeouts for IKEv2.

DNS records

  • DNS queries can be answered with a statically configured IP address.

SHDSL Port Monitoring

  • Triggering of events in the event of a change in status of the SHDSL port of the SCALANCE M826.

VRRPv3 Address Tracking

  • To enable redundant connections with several devices, the feature VRRPv3 with existing interface tracking has been extended to include IP and FQDN tracking.

Flashing of own LEDs

  • The LEDs of own module group can be made to flash under DCP Discovery.

 

 

Corrections were made in the following areas: 

Digital output

  • The digital output can be used to signal an active VPN connection, e.g. to a SINEMA RC server.

SNMPv3 Authentication Error

  • SNMPv3 connections are possible with AES128 encryption.

 

 

Security information: 

This update contains security-relevant changes which enhance robustness against possible attacks. We therefore recommend you update the firmware. 

Security fixes and improvements:  

  • Correction for SSA-809841: Buffer Overflow Vulnerability in Third-Party Component pppd

 

Firmware update V6.3 has been released for upgrading the following product versions:  

SCALANCE M804PB

6GK5804-0AP00-2AA2

SCALANCE M812-1 (ANNEX A)

6GK5812-1AA00-2AA2

SCALANCE M812-1 (ANNEX B)

6GK5812-1BA00-2AA2

SCALANCE M816-1 (ANNEX A)

6GK5816-1AA00-2AA2

SCALANCE M816-1 (ANNEX B)

6GK5816-1BA00-2AA2

SCALANCE M826-2

6GK5826-2AB00-2AB2

SCALANCE M874-2

6GK5874-2AA00-2AA2

SCALANCE M874-3

6GK5874-3AA00-2AA2

SCALANCE M874-3 (CN)

6GK5874-3AA00-2FA2

SCALANCE M876-3

6GK5876-3AA02-2BA2

SCALANCE M876-3 (ROK)

6GK5876-3AA02-2EA2

SCALANCE M876-4 (EU)

6GK5876-4AA00-2BA2

SCALANCE M876-4 (NAM)

6GK5876-4AA00-2DA2

SCALANCE S615

6GK5615-0AA00-2AA2

RUGGEDCOM RM1224 LTE(4G) EU

6GK6 108-4AM00-2BA2

RUGGEDCOM RM1224 LTE(4G) NAM

6GK6 108-4AM00-2DA2

 

 

Third-party software – license conditions and copyright information

You can find the copyright notes on the third-party software included in this product, especially Open Source Software, as well as applicable license conditions for this type of third-party software in the file ReadMe_OSS.

Special note for resellers

The information and the license conditions in the Readme_OSS file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.
   OSS_SCALANCE-M-800-S615_86.pdf (12.2 MB)

Please read the notes on installation in the product documentation.

 

You can download the file here.

 Download unterliegt Exportcontrolle  SCALANCE_M800_S615_V06.03.00_18.01_estc.zip (21.4 MB)

Hash:  Registrierung notwendig  V6.3_Hash_256.txt (1 KB)

You can download the private MIB here.

 Registrierung notwendig  scalance_m_msps.zip (163.6 KB)

Hash:  Registrierung notwendig  msps_Hash_256.txt (1 KB)

 

You can find the source code of the Open Source Software here:

 Download unterliegt Exportcontrolle  M800_S615_V06.03.00_oss.zip (211.1 MB) 

Hash:  Registrierung notwendig  Hash_256.txt (1 KB) 

 

 

 

Contact for technical issues: Customer Support, DI CS SD CCC TS, Contact form

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.