×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109781152, Entry date: 08/20/2020
(0)
Rate

Sales and delivery release SIMATIC Safe Kinematics V2.0

  • Entry
  • Associated product(s)
As of now the product SIMATIC Safe Kinematics V2.0 is available for sale and delivery.
As of now the product SIMATIC Safe Kinematics V2.0 is available for sale and delivery.

With SIMATIC Safe Kinematics, movement in space of predefined kinematics with up to 12 interpolating axes can be monitored safely. The following monitoring functions are available:
  • Safe velocity monitoring
    With safe velocity monitoring you monitor the cartesian velocity of individual kinematics points, e.g. at the Tool Center Point or at joints.
  • Safe zone monitoring
    With safe zone monitoring you monitor the position of the kinematics in the cartesian space, e.g. to limit the travel range of the kinematics or to monitor areas that can be entered by operating staff.
  • Safe orientation monitoring
    With safe orientation monitoring you monitor the orientation of the flange at an user-defined kinematics, e.g.  the operation on a workpiece may only be enabled if the tool is vertical to the floor.

The following kinematics are supported:
  • Cartesian portal 
  • Roller picker (vertical and horizontal)
  • Delta picker
  • SCARA
  • Articulated arm 
  • User-defined serial kinematic



SIMATIC Safe Kinematics V2.0 is an option package of the TIA Portal and is installed as a setup in TIA Portal V16 as of update 1.

The product contains a fail-safe function block library that must be integrated in the programming environment of STEP 7 Safety Advanced and connected on the input and output sides.

SIMATIC Safe Kinematics V2.0 supports the following PLCs:

  • CPU 1517F‑3 PN/DP with firmware version 2.8.x
  • CPU 1518F‑4 PN/DP with firmware version 2.8.x
  • CPU 1517TF‑3 PN/DP with firmware version 2.8.x
  • CPU 1515SP PC2 TF with CPU 1505SP TF with firmware version 20.8.x

 

Ordering data

SIMATIC Safe Kinematics V2.0 is available as a runtime option for the TIA Portal with article number 6ES7823-0FE01-1AA0.

The product can only be ordered via Online Software Delivery (OSD). The download includes the license certificate and an installation setup for the TIA Portal for SIMATIC Safe Kinematics.

 ProductArticle number 
 SIMATIC Safe Kinematics V2.0 6ES7823-0FE01-1AA0

 

System requirements

  • SIMATIC STEP 7 Professional (TIA Portal) V16 from update 1
  • STEP 7 Safety Advanced V16

SIMATIC Safe Kinematics requires SINAMICS S120 drives from firmware V5.1 with Safety Integrated Advanced Functions as a subordinated drive system.  


Further information

  • Function manual SIMATIC Safe Kinematics, see entry ID: 109762959 
  • Compatibility list, see entry ID: 109759466 












Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.