×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109782540, Entry date: 11/04/2020
(0)
Rate

Service Pack 2 for SIMATIC ODK 1500S V2.5 available

  • Entry
  • Associated product(s)
Service Pack 2 for SIMATIC ODK 1500S V2.5 is now available. It comprises a new template for C++ applications on CPU 1518 MFP V2.8

New functions

The service pack includes the following new functions:

  • New template "C++ Project for MFP Linux application (CPU 1518 MFP FW V2.8 or higher"
    The new template allows to develop C++ applications for CPU 1518 MFP Firmware Version V2.8 or higher. The Eclipse development environment required for this is included in the scope of delivery. Details on CPU 1518 MFP V2.8 are provided in the relevant delivery release 109782620

The new functions and improvements of the existing SP1 are integrated in SP2 and can be used, see product announcement  109773165 


Installation

The SIMATIC ODK 1500S V2.5.2 can be installed either as a standalone or via an existing V2.5 installation.

Download:  109774241 

A license for Version V2.5 is required to operate SIMATIC ODK 1500S V2.5.2

Installation is as follows:

  1. Download the setup files and the file including the SHA-256 checksums and store them in a directory.
  2. Check the setup files using the SHA-256 checksum
  3. Run the EXE file to start the setup.


Migration of existing C++ applications

If you want to continue to use C++ applications, which have been created for a firmware version <= V2.6, on CPU 1518 MFP V2.8, proceed as follows:

  1. Create a new project in Eclipse using the template "C++ Project for MFP Linux application (CPU 1518 MFP FW V2.8 or higher".
  2. Transfer the sources of our existing application to the new project.
  3. Generate the application anew and transfer it to CPU 1518 MFP V2.8


Security information

In order to protect technical infrastructure, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens products and solutions constitute one element of such a concept. You can find additional information about cybersecurity at
https://www.siemens.com/cybersecurity#Ouraspiration.
 
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.