×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109782919, Entry date: 06/28/2021
(2)
Rate

Release for delivery SINAMICS DCC V17

  • Entry
  • Associated product(s)
SINAMICS DCC V17 is available for delivery effective immediately. SINAMICS DCC V17 is the innovative technological enhancement of SINAMICS drives in the TIA Portal.

SINAMICS DCC (Drive Control Chart) is a technological enhancement of the SINAMICS S120/S150/G130/G150/MV drive systems and for SIMATIC Drive Controller. It enables the device functionality of the drive systems to be individually expanded with freely available closed-loop control, arithmetic and logic blocks. The user-friendly configuration tool facilitates easy graphical configuration of the blocks and their integration in the drive unit.

Through the Siemens application support, a series of application examples (winder, synchronous operation, cross-cutter, etc.) are available for download on the basis of SINAMICS DCC and can be deployed as a ready-to-use solution or be individually adapted or expanded.


SINAMICS DCC V17 is an option package for Startdrive Basic or Advanced V17 and has its own setup and own engineering license. The engineering license purchased for V17 is also valid for all older SINAMICS DCC versions.

You can find information about additional TIA Portal V17 products under 109784438 

Highlights SINAMICS DCC V17

The following new functions are available with SINAMICS DCC V17

  • Know-how protection for charts

  • Online engineering of the charts

    • Changing the value of a block connection online 

    • Inserting blocks into a DCC chart online 

    • Deleting blocks in the DCC chart online

    • Inserting block connections online 

    • Deleting block connections online 

    • Changing the run sequence of blocks online

  • Creating subcharts (partition)

  • Handling improvements: 

    • Switching over between the PIN name and the parameter text in the editor 

    • Zoom in/out with double click in the editor

    • Block search in the project library by entering the block name

    • Library update with block assignment

  • Support of additional function rights for changes to drive parameters for UMAC

  • Support of SINAMICS firmware V5.2 SP3

  • Support of SINAMICS Integrated in the SIMATIC Drive Controller

  • Support of CU320-2 DP 

Selection and ordering data

SINAMICS DCC V17 includes the "SINAMICS DCC combo V17" engineering license for simultaneously using
  • SINAMICS DCC V17 for Startdrive V17
  • SINAMICS DCC V3.3/3.4 for STARTER V5.3/V5.4 
    To use the engineering license "SINAMICS DCC combo V17" for SINAMICS DCC V3.3/V3.4, SINAMICS Startdrive V17 must be installed with SINAMICS DCC V17 in parallel on a PC.

 ProductDownload Article No.Article number, package (DVD)
SINAMICS DCC Combo V176SL3070-4HA01-0XG56SL3070-4HA01-0XA5 
SINAMICS DCC Combo V17 Upgrade
Upgrade V15...V16  -> V17

6SL3070-4HA01-0XK5

6SL3070-4HA01-0XE5 
SINAMICS DCC Combo Software Update Service

6SL3070-4AA01-0XY8

6SL3070-4AA01-0XL8 


Trial software download

Here, you can download the trial version for SINAMICS DCC V17 and test it for 21 days: 109782920 

System requirements

The recommended hardware and software are listed in the following table.

 Hardware/softwareRecommendation 
 Computer


SIMATIC FIELD PG M6 Comfort or higher (or comparable PC)


 Processor Intel® Core™ i5-8400H (2.5 to 4.2 GHz; 4 cores + Hyper-Threading; 8 MB Smart Cache)
 RAM 16 GB or more (32 GB for large projects)
 Hard disk SSD with at least 50 GB of available memory
 Monitor 15.6" Full HD display (1920 x 1080 or higher)
 Operating system

 Windows 10 (64-bit)

  • Windows 10 Professional Version 1909, 2004, 2009/20H2
  • Windows 10 Enterprise 1909, 2004, 2009/20H2
  • Windows 10 IoT Enterprise 2016 LTSB
  • Windows 10 IoT Enterprise 2019 LTSC

 Windows Server (64-bit)

  • Windows Server 2016 Standard (full installation)
  • Windows Server 2019 Standard (full installation)

Compatibility with other products

SINAMICS DCC V17

  • operates together with Startdrive V17, STEP 7 V17 and WinCC V17 in one framework.
  • Can be installed on one computer in parallel with another Startdrive version with SINAMICS DCC.
  • Can be installed on one computer in parallel to SINAMICS MICROMASTER STARTER V5.3 and SINAMICS DCC V3.3 and higher.

Important note

TIA Portal project version  V15.1...V16 are upgraded with TIA Portal V17 to project version V17. If you wish to work with or edit a TIA Portal project version V15.1...V16, we recommend an additional installation of the corresponding software for TIA Portal V17.

Supported virtualization platforms

  • VMware vSphere Hypervisor (ESXi) 6.7

  • VMware Workstation 15.5.0

  • VMware Player 15.5.0

  • Microsoft Hyper-V Server 2019


The following security programs are compatible with SINAMICS DCC V17:

  • Virus scanner
    • Symantec Endpoint Protection 14.2

    • Trend Micro Office Scan 12.0

    • McAfee Endpoint Security (ENS) 10.6

    • Kaspersky Endpoint Security 11.3

    • Windows Defender

    • Qihoo 360 "Safe Guard 12.1" + "Virus Scanner" 

  • Encryption software

    • Microsoft BitLocker

  • Host-based intrusion detection system:

    • McAfee Application Control 8.2

Supported languages

  • Default installation: English, German, Chinese (simplified)
  • Language packs: French, Italian, Spanish

Manual

The Configuration Manual for SINAMICS DCC V17 is available at 109776202.


Constraints

Constraints according to list of constraints under 109776202 


You can find additional product information about SINAMICS DCC on the marketing Internet page for SINAMICS Startdrive: www.siemens.com/startdrive. 
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.