×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109783707, Entry date: 10/01/2020
(0)
Rate

DTM: SIPART PS2 - HART - SITRANS DTM

  • Entry
  • Associated product(s)
Engineering ToolSITRANS DTM




Supported Firmware:≥ 5.03.00
EDD-Version:25.00.00
Order Number:6DR511*-0****-0*A*, 6DR512*-0****-0*A*,
6DR521*-0****-0*A*, 6DR521*-0****-0*A*
Firmware Version:5.03.00

To use this DTM package SITRANS DTM needs to be installed first. This is the Device Type Manager (DTM) for SIPART PS2 Profibus HART for FDT Frame applications (e.g. PactWare) with SITRANS DTM.

For more information please check:www.siemens.com/SIPARTPS2.

New features in this update:
- Pressure Sensor supported monitoring / diagnostics SITRANS DTM - powered by EDDL

This installation file requires the software SITRANS DTM. SITRANS DTM has to be installed only once and can be downloaded from product support under the following links:
SITRANS DTM 3.1: 53754140
SITRANS DTM 4.1: 109484287 replaced by SITRANS DTM 4.2: 109783560 

After the installation of SITRANS DTM, any desired device DTM can be installed. To install the device DTM, unzip it, then double-click on the .exe file and follow the instructions.
More information about the installation can be found under the following link: 61705616

 Registrierung notwendig  SIPART_PS2_HA_DTM_FDT_25_00_00_26.zip (1,1 MB)

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.