×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109792547, Entry date: 01/29/2021
(3)
Rate

TIA Portal V16 Add-In "SINAMICS G120X Basic Setup”

  • Entry
  • Associated product(s)
In pump and fan applications (e.g. water/wastewater or building technology) usually one PLC controls many drives. Often the configurations of this drives is nearly identic. Commissioning such systems for a great number of drives (>10) takes considerable time since it entails a repetitive process prone to errors. This TIA Portal Add-In enables the user to reduce commissioning time and effort.
The TIA Portal add-in "SINAMICS G120X Basic Setup" facilitates the commissioning of similar G120X drives by copying a desired configuration to one or many drive objects via the use of a PLC. 
From now on, you can enjoy of benefits, such as:
  • Reduced commissioning time and effort
  • Easy setup thanks to the user friendly interface
  • No drives parameters knowledge required
  • Error prevention with the help of automatic processing



The TIA Portal Add-in "SINAMICS G120X Basic Setup" offers the following functions:

  • User friendly wizards with graphical displays to input values
  • Display/selection of compatible drives in the project
  • Preparation of commissioning data offline and its backup (optional) on PC/PG in .xml format
  • Assignment of commissioning data to a single or more identical converter and storing the data in the PLC (as a local backup)
  • Execution of commissioning of one or more converters (mass commissioning) from PLC on demand using acyclic communication

Download
  Documentation (3,2 MB)
 Registrierung notwendig  TIA Portal V16 Add-In "SINAMICS G120X Basic Setup (3,8 MB)

Last Changes  
2021-04: Documentation V1.2: Changed chapter 3.1 "Add-ins installation" 


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.